Example MPC5777C eMIOS IGF test GHS614

Document created by Petr Stancik Employee on Aug 13, 2019
Version 1Show Document
  • View in full screen mode

********************************************************************************
* Detailed Description:
*
* eMIOS0 ch0 is set to SAIC mode generating interrupt on falling edge.
* The IGF ch16, connected to eMIOSch0, is set to filter low pulses <1.5us
* Intergation filter type is used for falling edge with given threshold.
* eMIOS interrupt is called if input signal low pulse is longer than 1.5us.
*
* ------------------------------------------------------------------------------
* Test HW: MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C
* MCU: PPC5777CMM03 2N45H CTZZS1521A
* Fsys: PLL1 = core_clk = 264MHz, PLL0 = 192MHz
* Debugger: Lauterbach Trace32
* Target: internal_FLASH
* Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A
* use USB connector (J21) on minimodule
*
* EVB connection: ETPUA30 (PortP P23-15) --> USER_LED_1 (P7-1)
* ETPUA31 (PortP P23-14) --> USER_LED_2 (P7-2)
*
* eMIOS ch0 (PortG P14-16)--> connect external pulse signal
*
********************************************************************************

1 person found this helpful

Outcomes