LS1088ARDB/LS1088ARDB-PB - How to update PBL/RCW binary on SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1088ARDB/LS1088ARDB-PB - How to update PBL/RCW binary on SD card

LS1088ARDB/LS1088ARDB-PB - How to update PBL/RCW binary on SD card

This how-to topic is applicable only for LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries on SD card.

Follow these steps to update the PBL/RCW binary on the SD card. 

Compiling PBL binary from RCW source file (optional)

If user already has a PBL binary, this step can be skipped.  

Clone the  rcw repository and compile the PBL binary. 

  1. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw
  2. $ cd rcw
  3. $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09 
  4. $ cd ls1088ardb
  5. If required, make changes to the rcw files.
  6. $ make

 

The default PBL binary for LS1088ARDB/LS1088ARDB-PB is FCQQQQQQQQ_PPP_H_0x1d_0x0d/rcw_1600_qspi.bin.  

See the rcw/ls1088ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files.

SD card start block number for PBL/RCW binary

Image SD card start block number
PBL/RCW binary0x00008 = 8

Refer the Flash layout for old boot flow with PPA – LSDK 18.09 and older releases for complete listing of the SD card start block numbers for all LSDK firmware images.

Programming PBL/RCW binary to SD card

  1. Plug the SD card into the Linux host.
  2. Run the following command on the Linux host:
    • $ sudo dd if=rcw_1600_qspi.bin of=/dev/sdX bs=512 seek=8 conv=fsync

      Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen.

      The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced.

      If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.

        
  3. Remove the SD card from the Linux host machine.
  4. On the LS1088ARDB/LS1088ARDB-PB, ensure that the switches are set to boot the board from the SD card. 
    • For booting from SD card, SW1[1:8] + SW2[1] = 0010_0000_0 
  5. Plug the SD card to the board and boot the board to Ubuntu.

If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.

Labels (1)
No ratings
Version history
Last update:
‎09-10-2020 01:59 AM
Updated by: