Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0

File uploaded by Martin Kovar Employee on Aug 23, 2016Last modified by Martin Kovar Employee on Apr 9, 2019
Version 2Show Document
  • View in full screen mode

********************************************************************************

* Detailed Description:

* This example shows, how to initialize FlexCAN modules for simple transmission

* and reception using RX interrupt. Both modules are configured for 100kbit/s

* bit rate. CAN_0 module transmits message using MB0. CAN_1 module receives

* message using interrupt via MB0.

*

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5748G-324DS, MPC574XG - Motherboard

* MCU:             PPC5748GMMN6A 1N81M

* Fsys:            PLL0 160MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  Connect jumpers J15 and J16 on motherboard

*                    Connect P14 H to P15 H

*                    Connect P14 L to P15 L

*

********************************************************************************

Outcomes