Example MPC5748G CRC32 GHS614

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5748G CRC32 GHS614

No ratings

Example MPC5748G CRC32 GHS614

********************************************************************************

* Detailed Description:

*

* This example shows how to use CRC module.

* - CRC32 is used

* - byte stream is written into input register

* - one test case uses direct access to CRC registers

* - second test case uses DMA to write the data stream

* - the results can be compared using this online calculator:

*   http://www.zorc.breitbandkatze.de/crc.html

* - screenshots from online calculator are attached

* ------------------------------------------------------------------------------

* Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C

* MCU:             PPC5748GMMN6A 1N81M

* Fsys:            160 MHz PLL

* Debugger:        Lauterbach Trace32

* Target:          internal_FLASH

********************************************************************************

Labels (1)
Attachments
Version history
Last update:
‎06-30-2016 12:20 AM
Updated by: