Example MPC5744P ETimerCountMode S32DS_1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5744P ETimerCountMode S32DS_1.0

Example MPC5744P ETimerCountMode S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL1 to maximum allowed freq. PLL1 is system frequency,

* PLL0 in initialized to 50MHz

* initializes peripherals clock (MOTC_CLK is set to 5MHz)

* initializes ETimer to count mode providing delay

* initializes interrupts, blinking one LED by ETimer interrupt,

*

*

*

* Test HW:         X-MPC5744PE257DC, MPC57xx motherboard

* MCU:             PPC5744PFMMM8 1N65H

* Fsys:            200 MHz

* Debugger:    Lauterbach Trace32

*                      PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  User LED 1 connected to A0 (P8.0),

*

*

* ------------------------------------------------------------------------------

Labels (1)
Attachments
No ratings
Version history
Last update:
‎01-12-2016 04:06 AM
Updated by: