Example MPC5604B PinToggleStationery CW210

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5604B PinToggleStationery CW210

Example MPC5604B PinToggleStationery CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt,

* initializes and display notice via UART terminal and then terminal ECHO.

* ------------------------------------------------------------------------------

* Test HW:        XPC5604B 100LQFP, XPC56XX EVB MOTHEBOARD Rev.C

* MCU:             PPC5604BE MLL 1M27V

* Fsys:             64/48 MHz

* Debugger:      Lauterbach Trace32

*                      PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH, (not enough memory for RAM target)

* Terminal:       19200-8-no parity-1 stop bit-no flow control on LINFLEX_0

* EVB connection: default

*

********************************************************************************

Labels (1)
Attachments
No ratings
Version history
Last update:
‎12-28-2015 02:55 AM
Updated by: