Example MPC5744P FlexPWM CTU SGEN triggering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5744P FlexPWM CTU SGEN triggering

Example MPC5744P FlexPWM CTU SGEN triggering

********************************************************************************

* Detailed Description:

*

*

* This example shows usage of FlexPWM and Sine Wave generator (SGEN) modules.

* The setting is selected in the way to have a PWM output signal synhronized with

* SWG output signal. This is necessary for resolver usage in motor control appls.

* The CTU_0 is triggered from FlexPWM_0's. The PMWB output rising edge is used here.

* The CTU generates the eTIMER1_TRG signal, that is a trigger signal for the

* SGEN module. The delay between PWMB and SGEN trigger is changed so you can see

* the generated sinusoidal signal change phase against the PWMB output.

*

* See attached Excel sheet for calculation of parammeters used here (AUX0_clk_DIV0,

* AUX0_clk_DIV1, SGEN_IOFREQ, PWM_PRESCALER, PWM_MODULO).

*

* This example is set for 9.765625KHz SGEN/PWM frequency.

*

* Note  because the SGEN trigger input is an asynchronous signal, it must be held high

* for at least 2 SGEN clock cycles in order to capture the input trigger.

* As the CTU generates the trigger as a pulse of single CTU clock width, the CTU clock must be

* half of the SGEN clock at least.

*

* Use the AUX0_clk_DIV0 to test this behaviour.

*

*

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

* EVB connection:

*

* P11.8 - D[7] .. SGEN output

*          connected to FEC PHY's MIIMODE input on motherboard,

*          to see full amplitude remove J26   

*

* P8.12    - A[11] .. FlexPWM A[0] output

* P8.11    - A[10] .. FlexPWM B[0] output

*

*

********************************************************************************

Labels (1)
Attachments
No ratings
Version history
Last update:
‎09-17-2015 01:16 AM
Updated by: