Example MPC5744P FlexPWM init with DMA reload

Document created by Petr Stancik Employee on Aug 13, 2015Last modified by ebiz_ws_prod on Dec 13, 2017
Version 3Show Document
  • View in full screen mode

********************************************************************************

* Detailed Description:

*

* This example shows usage of FlexPWM to generate independent

* PWM signals from Submodule0. The PWMX output is set for 50% duty.

* PWMA/PWMB outputs vary its duty cycles.

* The DMA module is used to reload VAL2-5 registers.

*

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  RAM, internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

* EVB connection:

* P8.12    - A[11] .. FlexPWM A[0] output

* P8.11    - A[10] .. FlexPWM B[0] output

* P11.10 - D[9] .. FlexPWM X[0] output

*

********************************************************************************

Original Attachment has been moved to: Example-MPC5744P-FlexPWM-Init-DMA-reload-GHS614.zip

2 people found this helpful

Attachments

    Outcomes