i.MX53 QSB Ubuntu Dual Display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 QSB Ubuntu Dual Display

i.MX53 QSB Ubuntu Dual Display

Enabling Dual Display in Ubuntu with the i.MX53 Quick Start Board


Here you will learn how to enable two displays in a Ubuntu system running in an iMX53 Quick Start Board.

We assume here that you already have a micro SD card with a valid Ubuntu image (including uboot, Linux kernel and Ubuntu filesystem).

You can use the original SD card that comes with the i.MX53 Quick Start Board, which brings an image of Ubuntu or, if you do not have the original SD card, you can reproduce it by downloading Ubuntu binaries package (L2.6.35_MX53_ER_1101_IMAGE) from Freescale iMX53qsb download area. You will also need to update U-boot and kernel binaries in the SD card with more recent images. You can find the most recent binaries (L2.6.35_MX53_ER_1109_IMAGE_) from Freescale iMX53qsb download area as well.

Introduction

To enable dual display, you need to perform two tasks:

  • Enable two displays at kernel level
  • Configure your Xorg server accordingly


Enabling Two Displays at Kernel Level

To enable two displays at kernel level means to map one display interface to fb0 device and the other to fb1 device. So first thing is to choose which interface will be the primary one, mapped as fb0. As an example, we consider the VGA interface as primary in this tutorial.

Second thing is to choose one of the other available external video interfaces to be secondary, mapped as fb1 device in the system. We consider the 4.3" seiko LCD display in this tutorial as the secondary interface.

Once chosen primary and secondary interfaces, we need to configure kernel video arguments accordingly. The arguments are available in specific variables in the U-boot that comes with the Ubuntu binaries. You can see them (HDMI, VGA, etc.) by printing the U-boot environment variables from the U-boot shell, but you will probably not find those variables in other versions of U-boot and their contents will probably need to be adapted to the kernel version in use, as arguments recognized by kernel modules varies considerably between kernel versions.

You can always refer to the Linux Release Notes documents for video arguments. It's available for each Linux BSP that can be found on the Freescale website. For the 1109 BSP, we have the following video arguments (extracted from i.MX53_START_Linux_BSP_Release_Note.pdf that comes with L2.6.35_11.09.01_ER_docs.tar.gz downloaded from here - IMX53_1109_LINUXDOCS_BUNDLE

  • VGA: video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga
  • SEIKO LCD: video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary

Both are considered primary, because these are the arguments for single display setups.

Now that we have video arguments for both desired interfaces, we only need to merge them together removing the primary argument from the one that is the secondary. In our case, we need to pass the following arguments to the kernel:

video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga video=mxcdi0fb:RGB24,SEIKO-WVGA 

For this, we can add these arguments to one of the variables that are used in the boot process. We can add the content to bootarg_base, for instance. In the U-boot command line, execute following commands to setup the environment:

setenv vga_and_seiko 'video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga video=mxcdi0fb:RGB24,SEIKO-WVGA' setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 vga_and_seiko' saveenv 

After applying a reset and booting the board, you shall have both interfaces enabled, but the secondary will not be used by the Xorg server until we complete the next step.


Configuring Xorg Server


Now that we have two video interfaces properly configured and mapped to /dev/fb0 and /dev/fb1 devices, we need to tell Xorg server how to use them.

Here is an example of xorg.conf file that you can use to replace the default one, found at /etc/X11:

Section "InputDevice" Identifier     "Generic Keyboard" Driver          "kbd" Option          "XkbRules"     "xorg" Option          "XkbModel"     "pc105" Option          "XkbLayout"     "us" EndSection  Section "InputDevice" Identifier     "Configured Mouse" Driver          "mouse" Option          "CorePointer" EndSection  Section "Device" Identifier     "i.MX Accelerated Framebuffer Device 0" Driver          "imx" Option          "fbdev"               "/dev/fb0"  # This option only recognized when "mxc_epdc_fb" frame buffer driver in # use.  Values are "RGB565" (default, 16-bit RGB), "Y8" (8-bit gray), # and "Y8INV" (8-bit gray inverted). Option          "FormatEPDC"               "Y8INV"  EndSection  Section "Device" Identifier     "i.MX Accelerated Framebuffer Device 1" Driver          "imx" Option          "fbdev"               "/dev/fb1"  EndSection  Section "Monitor" Identifier     "Configured Monitor 0" EndSection  Section "Monitor" Identifier     "Configured Monitor 1" EndSection  Section "Screen" Identifier     "Screen 0" Monitor          "Configured Monitor 0" Device          "i.MX Accelerated Framebuffer Device 0"  # These "Display" SubSection's are needed for working with the # "mxc_epdc_fb" frame buffer driver. SubSection     "Display" Depth     8 Visual     "StaticGray" EndSubSection SubSection     "Display" Depth     16 Visual     "TrueColor" EndSubSection EndSection  Section "Screen" Identifier     "Screen 1" Monitor          "Configured Monitor 1" Device          "i.MX Accelerated Framebuffer Device 1" EndSection  Section "ServerLayout" Identifier     "Xinerama Layout" Screen          "Screen 0" Screen          "Screen 1" RightOf "Screen 0" EndSection  Section "ServerFlags" Option          "Xinerama"          "true" EndSection 

Results

The following picture shows the i.MX 53 QSB running the extended desktop previously configured.

You can see the VGA monitor with a Firefox instance and the SEIKO LCD display with a calc instance.

IMX53QSBUbuntuDualDisplayExample.jpg


ラベル(1)
コメント

Hi

I want to use ubuntu with dual display on i.mx6q board.

And i what to use LVDS as the primary dispaly and use HDMI as the second one.

My u-boot's kernel parameters is bellow:

video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24

And my x window configure file is as bellow:

Section "InputDevice"

        Identifier      "Generic Keyboard"

        Driver          "kbd"

        Option          "XkbRules"      "xorg"

        Option          "XkbModel"      "pc105"

        Option          "XkbLayout"     "us"

EndSection

Section "InputDevice"

        Identifier      "Configured Mouse"

        Driver          "mouse"

        Option          "CorePointer"

EndSection

Section "Device"

        Identifier      "LVDS"

       Driver          "vivante"

        Option          "fbdev"         "/dev/fb0"

       Option          "vivante_fbdev" "/dev/fb0"

       Option          "HWcursor"      "false"

EndSection

Section "Device"

        Identifier      "HDMI"

        Driver          "fbdev"                        ///////////////  If i use "vivante", X window start will failed, it seems that "vivante" not support two display?

        Option          "fbdev"         "/dev/fb2"

EndSection

Section "Monitor"

        Identifier      "LVDS Monitor"

EndSection

Section "Monitor"

        Identifier      "HDMI Monitor"

EndSection

Section "Screen"

        Identifier      "LVDS Screen"

        Monitor         "LVDS Monitor"

        Device          "LVDS"

EndSection

Section "Screen"

        Identifier      "HDMI Screen"

        Monitor         "HDMI Monitor"

        Device          "HDMI"

EndSection

Section "ServerLayout"

        Identifier      "Dual Layout"

        Screen 0        "LVDS Screen"

        Screen 1        "HDMI Screen" RightOf "LVDS Screen"

        Option          "Xinerama"  "on"

EndSection

Then i get the two display worked, But somthing is wrong.

On the left of HDMI display there is a copy of lvds.

Is my settings wrong?

Do you know about this?

Thank you

LVDS.jpgHDMI.jpg

%3CLINGO-SUB%20id%3D%22lingo-sub-1115111%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3Ei.MX53%20QSB%20Ubuntu%20Dual%20Display%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1115111%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CH1%20id%3D%22toc-hId-381558444%22%20id%3D%22toc-hId-381558444%22%20id%3D%22toc-hId-1304222357%22%3E%3CSPAN%20class%3D%22mw-headline%22%3EUbuntu%E3%81%A7i.MX53%E3%82%AF%E3%82%A4%E3%83%83%E3%82%AF%E3%82%B9%E3%82%BF%E3%83%BC%E3%83%88%E3%83%9C%E3%83%BC%E3%83%89%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%83%87%E3%83%A5%E3%82%A2%E3%83%AB%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%92%E6%9C%89%E5%8A%B9%E3%81%AB%E3%81%99%E3%82%8B%3C%2FSPAN%3E%3C%2FH1%3E%3CP%3E%3CSPAN%20class%3D%22mw-headline%22%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%E3%81%93%E3%81%93%E3%81%A7%E3%81%AF%E3%80%81iMX53%20%3CA%20href%3D%22http%3A%2F%2Fwww.imxdev.org%2Fwiki%2Findex.php%3Ftitle%3DI.MX53_QSB_Ubuntu_Dual_Display%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%20style%3D%22text-decoration%3A%20underline%3B%22%20title%3D%22Powered%20by%20Text-Enhance%22%20target%3D%22_blank%22%3E%E3%82%AF%E3%82%A4%E3%83%83%E3%82%AF%E3%82%B9%E3%82%BF%E3%83%BC%E3%83%88%E3%83%9C%E3%83%BC%E3%83%89%3C%2FA%3E%20%E3%81%A7%E5%AE%9F%E8%A1%8C%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8BUbuntu%E3%82%B7%E3%82%B9%E3%83%86%E3%83%A0%E3%81%A72%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%92%E6%9C%89%E5%8A%B9%E3%81%AB%E3%81%99%E3%82%8B%E6%96%B9%E6%B3%95%E3%82%92%E5%AD%A6%E7%BF%92%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%E3%81%93%E3%81%93%E3%81%A7%E3%81%AF%E3%80%81%E6%9C%89%E5%8A%B9%E3%81%AAUbuntu%E3%82%A4%E3%83%A1%E3%83%BC%E3%82%B8(uboot%E3%80%81Linux%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%80%81Ubuntu%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%82%B7%E3%82%B9%E3%83%86%E3%83%A0%E3%82%92%E5%90%AB%E3%82%80)%E3%82%92%E5%82%99%E3%81%88%E3%81%9F%E3%83%9E%E3%82%A4%E3%82%AF%E3%83%ADSD%E3%82%AB%E3%83%BC%E3%83%89%E3%81%8C%E3%81%99%E3%81%A7%E3%81%AB%E3%81%82%E3%82%8B%E3%81%93%E3%81%A8%E3%82%92%E5%89%8D%E6%8F%90%E3%81%A8%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3Ei.MX53%E3%82%AF%E3%82%A4%E3%83%83%E3%82%AF%E3%82%B9%E3%82%BF%E3%83%BC%E3%83%88%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E4%BB%98%E5%B1%9E%E3%81%AE%E3%82%AA%E3%83%AA%E3%82%B8%E3%83%8A%E3%83%AB%E3%81%AESD%E3%82%AB%E3%83%BC%E3%83%89%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6Ubuntu%E3%81%AE%E3%82%A4%E3%83%A1%E3%83%BC%E3%82%B8%E3%82%92%E8%A1%A8%E7%A4%BA%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%82%82%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%81%97%E3%80%81%E3%82%AA%E3%83%AA%E3%82%B8%E3%83%8A%E3%83%AB%E3%81%AESD%E3%82%AB%E3%83%BC%E3%83%89%E3%81%8C%E3%81%AA%E3%81%84%E5%A0%B4%E5%90%88%E3%81%AF%E3%80%81%3CA%20class%3D%22text%20external%22%20href%3D%22http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Fprod_summary.jsp%3Fcode%3DIMX53QSB%26amp%3Bfpsp%3D1%26amp%3Btab%3DDesign_Tools_Tab%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%20target%3D%22_blank%22%3E%20Freescale%20iMX53qsb%E3%81%AE%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%E3%82%A8%E3%83%AA%E3%82%A2%3C%2FA%3E%20%E3%81%8B%E3%82%89Ubuntu%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%83%91%E3%83%83%E3%82%B1%E3%83%BC%E3%82%B8(%3CA%20class%3D%22text%20external%22%20href%3D%22https%3A%2F%2Fwww.freescale.com%2Fwebapp%2FDownload%3FcolCode%3DL2.6.35_MX53_ER_1101_IMAGE%26amp%3BappType%3Dlicense%26amp%3Blocation%3Dnull%26amp%3Bfpsp%3D1%26amp%3BWT_TYPE%3DBoard%2520Support%2520Packages%26amp%3BWT_VENDOR%3DFREESCALE%26amp%3BWT_FILE_FORMAT%3Dgz%26amp%3BWT_ASSET%3DDownloads%26amp%3Bsr%3D8%26amp%3BParent_nodeId%3D1298413274207729722207%26amp%3BParent_pageType%3Dproduct%26amp%3BParent_nodeId%3D1298413274207729722207%26amp%3BParent_pageType%3Dproduct%26amp%3BParent_nodeId%3D1298413274207729722207%26amp%3BParent_pageType%3Dproduct%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%20target%3D%22_blank%22%3E%20L2.6.35_MX53_ER_1101_IMAGE)%E3%82%92%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%E3%81%97%E3%81%A6%E5%86%8D%E7%8F%BE%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FA%3E%E3%81%BE%E3%81%9F%E3%80%81SD%E3%82%AB%E3%83%BC%E3%83%89%E5%86%85%E3%81%AEU-boot%E3%81%A8%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%82%92%E6%9C%80%E6%96%B0%E3%81%AE%E3%82%A4%E3%83%A1%E3%83%BC%E3%82%B8%E3%81%A7%E6%9B%B4%E6%96%B0%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E6%9C%80%E6%96%B0%E3%81%AE%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%20(L2.6.35_MX53_ER_1109_IMAGE_)%20%E3%81%AF%20%3CA%20class%3D%22text%20external%22%20href%3D%22http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Fprod_summary.jsp%3Fcode%3DIMX53QSB%26amp%3Bfpsp%3D1%26amp%3Btab%3DDesign_Tools_Tab%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%20target%3D%22_blank%22%3E%E3%80%81Freescale%20iMX53qsb%20%E3%81%AE%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%20%E3%82%A8%E3%83%AA%E3%82%A2%3C%2FA%3E%20%E3%81%8B%E3%82%89%E3%82%82%E8%A6%8B%E3%81%A4%E3%81%91%E3%82%8B%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId-1072119918%22%20id%3D%22toc-hId-1072119918%22%20id%3D%22toc-hId-1994783831%22%3E%3CSPAN%20class%3D%22mw-headline%22%3E%20%E3%81%AF%E3%81%98%E3%82%81%E3%81%AB%20%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%83%87%E3%83%A5%E3%82%A2%E3%83%AB%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%92%E6%9C%89%E5%8A%B9%E3%81%AB%E3%81%99%E3%82%8B%E3%81%AB%E3%81%AF%E3%80%81%E6%AC%A1%E3%81%AE2%E3%81%A4%E3%81%AE%E3%82%BF%E3%82%B9%E3%82%AF%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CUL%3E%3CLI%3E%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%AC%E3%83%99%E3%83%AB%E3%81%A7%E3%81%AE%202%20%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%AE%E6%9C%89%E5%8A%B9%E5%8C%96%3C%2FLI%3E%3CLI%3E%E3%81%9D%E3%82%8C%E3%81%AB%E5%BF%9C%E3%81%98%E3%81%A6%20Xorg%20%E3%82%B5%E3%83%BC%E3%83%90%E3%83%BC%E3%82%92%E8%A8%AD%E5%AE%9A%E3%81%97%E3%81%BE%E3%81%99%3C%2FLI%3E%3C%2FUL%3E%3CH2%20id%3D%22toc-hId--735334545%22%20id%3D%22toc-hId--735334545%22%20id%3D%22toc-hId-187329368%22%3E%3CSPAN%20class%3D%22mw-headline%22%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FH2%3E%3CH2%20id%3D%22toc-hId-1752178288%22%20id%3D%22toc-hId-1752178288%22%20id%3D%22toc-hId--1620125095%22%3E%3CSPAN%20class%3D%22mw-headline%22%3E%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%AC%E3%83%99%E3%83%AB%E3%81%A7%E3%81%AE%202%20%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%AE%E6%9C%89%E5%8A%B9%E5%8C%96%20%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%AC%E3%83%99%E3%83%AB%E3%81%A7%202%20%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%92%E6%9C%89%E5%8A%B9%E3%81%AB%E3%81%99%E3%82%8B%E3%81%A8%E3%81%84%E3%81%86%E3%81%93%E3%81%A8%E3%81%AF%E3%80%811%20%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%82%92%20fb0%20%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%AB%E3%83%9E%E3%83%83%E3%83%97%E3%81%97%E3%80%81%E3%82%82%E3%81%86%201%20%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%82%92%20fb1%20%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%AB%E3%83%9E%E3%83%83%E3%83%97%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%82%92%E6%84%8F%E5%91%B3%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%97%E3%81%9F%E3%81%8C%E3%81%A3%E3%81%A6%E3%80%81%E6%9C%80%E5%88%9D%E3%81%AB%E3%80%81fb0%20%E3%81%A8%E3%81%97%E3%81%A6%E3%83%9E%E3%83%83%E3%83%97%E3%81%95%E3%82%8C%E3%81%9F%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%82%92%E9%81%B8%E6%8A%9E%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E4%BE%8B%E3%81%A8%E3%81%97%E3%81%A6%E3%80%81%E3%81%93%E3%81%AE%E3%83%81%E3%83%A5%E3%83%BC%E3%83%88%E3%83%AA%E3%82%A2%E3%83%AB%E3%81%A7%E3%81%AFVGA%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%82%92%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%E3%81%A8%E8%A6%8B%E3%81%AA%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E6%AC%A1%E3%81%AB%E3%80%81%E4%BB%96%E3%81%AE%E4%BD%BF%E7%94%A8%E5%8F%AF%E8%83%BD%E3%81%AA%E5%A4%96%E9%83%A8%E3%83%93%E3%83%87%E3%82%AA%20%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%81%AE%201%20%E3%81%A4%E3%82%92%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%81%A8%E3%81%97%E3%81%A6%E9%81%B8%E6%8A%9E%E3%81%97%E3%80%81%E3%82%B7%E3%82%B9%E3%83%86%E3%83%A0%E5%86%85%E3%81%A7%20fb1%20%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%A8%E3%81%97%E3%81%A6%E3%83%9E%E3%83%83%E3%83%94%E3%83%B3%E3%82%B0%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%81%AE%E3%83%81%E3%83%A5%E3%83%BC%E3%83%88%E3%83%AA%E3%82%A2%E3%83%AB%E3%81%A7%E3%81%AF%E3%80%814.3%E3%82%A4%E3%83%B3%E3%83%81%E3%81%AE%E3%82%BB%E3%82%A4%E3%82%B3%E3%83%BCLCD%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%92%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%81%A8%E8%A6%8B%E3%81%AA%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%81%A8%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%82%92%E9%81%B8%E6%8A%9E%E3%81%97%E3%81%9F%E3%82%89%E3%80%81%E3%81%9D%E3%82%8C%E3%81%AB%E5%BF%9C%E3%81%98%E3%81%A6%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%93%E3%83%87%E3%82%AA%E5%BC%95%E6%95%B0%E3%82%92%E8%A8%AD%E5%AE%9A%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E5%BC%95%E6%95%B0%E3%81%AF%E3%80%81Ubuntu%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%81%AB%E4%BB%98%E5%B1%9E%E3%81%99%E3%82%8BU-boot%E3%81%AE%E7%89%B9%E5%AE%9A%E3%81%AE%E5%A4%89%E6%95%B0%E3%81%A7%E4%BD%BF%E7%94%A8%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%81%9D%E3%82%8C%E3%82%89%20(HDMI%E3%80%81VGA%20%E3%81%AA%E3%81%A9)%20%E3%81%AF%E3%80%81U-boot%20%E3%82%B7%E3%82%A7%E3%83%AB%E3%81%8B%E3%82%89%20U-boot%20%E7%92%B0%E5%A2%83%E5%A4%89%E6%95%B0%E3%82%92%E5%87%BA%E5%8A%9B%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%A7%E7%A2%BA%E8%AA%8D%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E4%BB%96%E3%81%AE%E3%83%90%E3%83%BC%E3%82%B8%E3%83%A7%E3%83%B3%E3%81%AE%20U-boot%20%E3%81%A7%E3%81%AF%E3%81%93%E3%82%8C%E3%82%89%E3%81%AE%E5%A4%89%E6%95%B0%E3%81%AF%E3%81%8A%E3%81%9D%E3%82%89%E3%81%8F%E8%A6%8B%E3%81%A4%E3%81%8B%E3%82%89%E3%81%9A%E3%80%81%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%81%8C%E8%AA%8D%E8%AD%98%E3%81%99%E3%82%8B%E5%BC%95%E6%95%B0%E3%81%AF%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%90%E3%83%BC%E3%82%B8%E3%83%A7%E3%83%B3%E9%96%93%E3%81%A7%E3%81%8B%E3%81%AA%E3%82%8A%E7%95%B0%E3%81%AA%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E3%81%9D%E3%81%AE%E5%86%85%E5%AE%B9%E3%81%AF%E4%BD%BF%E7%94%A8%E4%B8%AD%E3%81%AE%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%90%E3%83%BC%E3%82%B8%E3%83%A7%E3%83%B3%E3%81%AB%E9%81%A9%E5%90%88%E3%81%95%E3%81%9B%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8B%E3%81%A7%E3%81%97%E3%82%87%E3%81%86%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%83%93%E3%83%87%E3%82%AA%E5%BC%95%E6%95%B0%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E3%81%AF%E3%80%81%E3%81%84%E3%81%A4%E3%81%A7%E3%82%82%20Linux%20%E3%83%AA%E3%83%AA%E3%83%BC%E3%82%B9%E3%83%8E%E3%83%BC%E3%83%88%E3%81%AE%E3%83%89%E3%82%AD%E3%83%A5%E3%83%A1%E3%83%B3%E3%83%88%E3%82%92%E5%8F%82%E7%85%A7%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%82%8C%E3%81%AF%E3%80%81Freescale%20%E3%81%AE%20Web%20%E3%82%B5%E3%82%A4%E3%83%88%E3%81%AB%E3%81%82%E3%82%8B%E5%90%84%20Linux%20BSP%20%E3%81%A7%E4%BD%BF%E7%94%A8%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%821109%20BSP%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E3%81%AF%E3%80%81%E6%AC%A1%E3%81%AE%E3%83%93%E3%83%87%E3%82%AA%E5%BC%95%E6%95%B0%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99(%20%3CA%20class%3D%22text%20external%22%20href%3D%22http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Fprod_summary.jsp%3Fcode%3DIMX53QSB%26amp%3Bfpsp%3D1%26amp%3Btab%3DDocumentation_Tab%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%20target%3D%22_blank%22%3E%E3%81%93%E3%81%93%E3%81%8B%E3%82%89%3C%2FA%3E%20%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%E3%81%97%E3%81%9FL2.6.35_11.09.01_ER_docs.tar.gz%E3%81%AB%E4%BB%98%E5%B1%9E%E3%81%AEi.MX53_START_Linux_BSP_Release_Note.pdf%E3%81%8B%E3%82%89%E6%8A%9C%E7%B2%8B%20%3CA%20class%3D%22text%20external%22%20href%3D%22https%3A%2F%2Fwww.freescale.com%2Fwebapp%2FDownload%3FcolCode%3DIMX53_1109_LINUXDOCS_BUNDLE%26amp%3Blocation%3Dnull%26amp%3Bfpsp%3D1%26amp%3BParent_nodeId%3D1298413274207729722207%26amp%3BParent_pageType%3Dproduct%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%20target%3D%22_blank%22%3EIMX53_1109_LINUXDOCS_BUNDLE%3C%2FA%3E%3CLI-EMOJI%20id%3D%22lia_disappointed-face%22%20title%3D%22%3Adisappointed_face%3A%22%3E%3C%2FLI-EMOJI%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CUL%3E%3CLI%3EVGA%3A%20video%3Dmxcdi1fb%3AGBR24%2CVGA-XGA%20di1_primary%20vga%3C%2FLI%3E%3CLI%3ESEIKO%20LCD%3A%20video%3Dmxcdi0fb%3ARGB24%2CSEIKO-WVGA%20di0_primary%3C%2FLI%3E%3C%2FUL%3E%3CP%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CDIV%20style%3D%22background-color%3A%20%23eeeeff%3B%20padding-left%3A%2030px%3B%20width%3A%2060%25%3B%20margin-left%3A%2020%25%3B%22%3E%3CP%3E%E3%81%93%E3%82%8C%E3%82%89%E3%81%AF%E5%8D%98%E4%B8%80%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E8%A8%AD%E5%AE%9A%E3%81%AE%E5%BC%95%E6%95%B0%E3%81%A7%E3%81%82%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E3%81%A9%E3%81%A1%E3%82%89%E3%82%82%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%E3%81%A8%E8%A6%8B%E3%81%AA%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3C%2FDIV%3E%3CP%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E5%BF%85%E8%A6%81%E3%81%AA%E4%B8%A1%E6%96%B9%E3%81%AE%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%81%AE%E3%83%93%E3%83%87%E3%82%AA%E5%BC%95%E6%95%B0%E3%81%8C%E7%94%A8%E6%84%8F%E3%81%A7%E3%81%8D%E3%81%9F%E3%81%AE%E3%81%A7%E3%80%81%E3%81%9D%E3%82%8C%E3%82%89%E3%82%92%E3%83%9E%E3%83%BC%E3%82%B8%E3%81%97%E3%81%A6%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%81%A7%E3%81%82%E3%82%8B%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%81%8B%E3%82%89%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%E5%BC%95%E6%95%B0%E3%82%92%E5%89%8A%E9%99%A4%E3%81%99%E3%82%8B%E3%81%A0%E3%81%91%E3%81%A7%E6%B8%88%E3%81%BF%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%81%AE%E5%A0%B4%E5%90%88%E3%80%81%E6%AC%A1%E3%81%AE%E5%BC%95%E6%95%B0%E3%82%92%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%81%AB%E6%B8%A1%E3%81%99%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CPRE%20class%3D%22jive-pre%22%3Evideo%3Dmxcdi1fb%3AGBR24%2CVGA-XGA%20di1_primary%20vga%20video%3Dmxcdi0fb%3ARGB24%2CSEIKO-WVGA%20%3C%2FPRE%3E%3CP%3E%E3%81%93%E3%81%AE%E3%81%9F%E3%82%81%E3%81%AB%E3%80%81%E3%83%96%E3%83%BC%E3%83%88%E3%83%97%E3%83%AD%E3%82%BB%E3%82%B9%E3%81%A7%E4%BD%BF%E7%94%A8%E3%81%95%E3%82%8C%E3%82%8B%E5%A4%89%E6%95%B0%E3%81%AE1%E3%81%A4%E3%81%AB%E3%81%93%E3%82%8C%E3%82%89%E3%81%AE%E5%BC%95%E6%95%B0%E3%82%92%E8%BF%BD%E5%8A%A0%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%81%9F%E3%81%A8%E3%81%88%E3%81%B0%E3%80%81bootarg_base%E3%81%AB%E3%82%B3%E3%83%B3%E3%83%86%E3%83%B3%E3%83%84%E3%82%92%E8%BF%BD%E5%8A%A0%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82U-boot%20%E3%82%B3%E3%83%9E%E3%83%B3%E3%83%89%E3%83%A9%E3%82%A4%E3%83%B3%E3%81%A7%E3%80%81%E6%AC%A1%E3%81%AE%E3%82%B3%E3%83%9E%E3%83%B3%E3%83%89%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%97%E3%81%A6%E7%92%B0%E5%A2%83%E3%82%92%E3%82%BB%E3%83%83%E3%83%88%E3%82%A2%E3%83%83%E3%83%97%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CPRE%20class%3D%22jive-pre%22%3Esetenv%20vga_and_seiko%20'video%3Dmxcdi1fb%3AGBR24%2CVGA-XGA%20di1_primary%20vga%20video%3Dmxcdi0fb%3ARGB24%2CSEIKO-WVGA'%20setenv%20bootargs_base%20'setenv%20bootargs%20console%3Dttymxc0%2C115200%20vga_and_seiko'%20saveenv%20%3C%2FPRE%3E%3CP%3E%E3%83%AA%E3%82%BB%E3%83%83%E3%83%88%E3%82%92%E9%81%A9%E7%94%A8%E3%81%97%E3%81%A6%E3%83%9C%E3%83%BC%E3%83%89%E3%82%92%E8%B5%B7%E5%8B%95%E3%81%97%E3%81%9F%E5%BE%8C%E3%80%81%E4%B8%A1%E6%96%B9%E3%81%AE%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%E3%81%8C%E6%9C%89%E5%8A%B9%E3%81%AB%E3%81%AA%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E6%AC%A1%E3%81%AE%E3%82%B9%E3%83%86%E3%83%83%E3%83%97%E3%82%92%E5%AE%8C%E4%BA%86%E3%81%99%E3%82%8B%E3%81%BE%E3%81%A7%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%81%AF%20Xorg%20%E3%82%B5%E3%83%BC%E3%83%90%E3%83%BC%E3%81%AB%E3%82%88%E3%81%A3%E3%81%A6%E4%BD%BF%E7%94%A8%E3%81%95%E3%82%8C%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FP%3E%3CH2%20id%3D%22toc-hId--55276175%22%20id%3D%22toc-hId--55276175%22%20id%3D%22toc-hId-867387738%22%3E%3CSPAN%20class%3D%22mw-headline%22%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FH2%3E%3CH2%20id%3D%22toc-hId--1862730638%22%20id%3D%22toc-hId--1862730638%22%20id%3D%22toc-hId--940066725%22%3E%3CSPAN%20class%3D%22mw-headline%22%3EXorg%20%E3%82%B5%E3%83%BC%E3%83%90%E3%83%BC%E3%81%AE%E8%A8%AD%E5%AE%9A%3C%2FSPAN%3E%3C%2FH2%3E%3CH2%20id%3D%22toc-hId-624782195%22%20id%3D%22toc-hId-624782195%22%20id%3D%22toc-hId-1547446108%22%3E%3CSPAN%20class%3D%22mw-headline%22%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E2%E3%81%A4%E3%81%AE%E3%83%93%E3%83%87%E3%82%AA%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%E3%81%8C%E9%81%A9%E5%88%87%E3%81%AB%E8%A8%AD%E5%AE%9A%E3%81%95%E3%82%8C%E3%80%81%2Fdev%2Ffb0%20%E3%81%A8%20%2Fdev%2Ffb1%20%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%AB%E3%83%9E%E3%83%83%E3%83%94%E3%83%B3%E3%82%B0%E3%81%95%E3%82%8C%E3%81%9F%E3%81%AE%E3%81%A7%E3%80%81%E3%81%9D%E3%82%8C%E3%82%89%E3%81%AE%E4%BD%BF%E7%94%A8%E6%96%B9%E6%B3%95%E3%82%92%20Xorg%20%E3%82%B5%E3%83%BC%E3%83%90%E3%83%BC%E3%81%AB%E6%8C%87%E7%A4%BA%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%E4%BB%A5%E4%B8%8B%E3%81%AF%E3%80%81%2Fetc%2FX11%20%E3%81%AB%E3%81%82%E3%82%8B%E3%83%87%E3%83%95%E3%82%A9%E3%83%AB%E3%83%88%E3%81%AE%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%82%92%E7%BD%AE%E3%81%8D%E6%8F%9B%E3%81%88%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E4%BD%BF%E7%94%A8%E3%81%A7%E3%81%8D%E3%82%8B%20xorg.conf%20%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%81%AE%E4%BE%8B%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CPRE%20class%3D%22jive-pre%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22InputDevice%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22%E6%B1%8E%E7%94%A8%E3%82%AD%E3%83%BC%E3%83%9C%E3%83%BC%E3%83%89%22%20%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%20%22kbd%22%20%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22XkbRules%22%20%22xorg%22%20%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22XkbModel%22%20%22pc105%22%20%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22XkbLayout%22%20%22us%22%20EndSection%20Section%20%22InputDevice%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22Configured%20Mouse%22%20%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%20%22mouse%22%20%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22CorePointer%22%20EndSection%20Section%20%22%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%22%20%E8%AD%98%E5%88%A5%E5%AD%90%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%22i.MX%20Accelerated%20Framebuffer%20Device%200%22%20driver%20%22imx%22%20Option%20%22fbdev%22%20%22%2Fdev%2Ffb0%22%20%23%20%E3%81%93%E3%81%AE%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AFmxc_epdc_fb%E3%80%81%E3%83%95%E3%83%AC%E3%83%BC%E3%83%A0%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%81%8C%20%23%20%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E5%A0%B4%E5%90%88%E3%81%AB%E3%81%AE%E3%81%BF%E8%AA%8D%E8%AD%98%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E5%80%A4%E3%81%AF%E3%80%8CRGB565%E3%80%8D(%E3%83%87%E3%83%95%E3%82%A9%E3%83%AB%E3%83%88%3A16%E3%83%93%E3%83%83%E3%83%88RGB)%E3%80%81%E3%80%8CY8%E3%80%8D(8%E3%83%93%E3%83%83%E3%83%88%E3%82%B0%E3%83%AC%E3%83%BC)%E3%80%81%E3%80%8C%23%E3%80%8D%E3%81%8A%E3%82%88%E3%81%B3%E3%80%8CY8INV%E3%80%8D(8%E3%83%93%E3%83%83%E3%83%88%E3%82%B0%E3%83%AC%E3%83%BC%E5%8F%8D%E8%BB%A2)%E3%81%A7%E3%81%99%E3%80%82%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22FormatEPDC%22%20%22Y8INV%22%20EndSection%20Section%20%22%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22i.MX%20Accelerated%20Framebuffer%20Device%201%22%20Driver%20%22imx%22%20Option%20%22fbdev%22%20%22%2Fdev%2Ffb1%22%20EndSection%20Section%20%22Monitor%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22Configured%20Monitor%200%22%20EndSection%20Section%20%22Monitor%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22Configured%20Monitor%201%22%20EndSection%20Section%20%22Screen%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22Screen%200%22%20Monitor%20%22Configured%20Monitor%200%22%20Device%20%22i.MX%20Accelerated%20Framebuffer%20Device%200%22%20%23%20%E3%81%93%E3%82%8C%E3%82%89%E3%81%AE%20%22Display%22%20%E3%82%B5%E3%83%96%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AF%E3%80%81%23%20%22mxc_epdc_fb%22%20%E3%83%95%E3%83%AC%E3%83%BC%E3%83%A0%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E5%BF%85%E8%A6%81%E3%81%A7%E3%81%99%E3%80%82%E3%82%B5%E3%83%96%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22%E8%A1%A8%E7%A4%BA%22%20%E6%B7%B1%E5%BA%A6%208%20%E3%83%93%E3%82%B8%E3%83%A5%E3%82%A2%E3%83%AB%20%22StaticGray%22%20EndSubSection%20%E3%82%B5%E3%83%96%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%22%20%E6%B7%B1%E5%BA%A6%2016%20%E3%83%93%E3%82%B8%E3%83%A5%E3%82%A2%E3%83%AB%20%22TrueColor%22%20EndSubSection%20EndSection%20Section%20%22%E7%94%BB%E9%9D%A2%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22%E7%94%BB%E9%9D%A2%201%22%20%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%20%22%E6%A7%8B%E6%88%90%E6%B8%88%E3%81%BF%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%201%22%20%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%20%22i.MX%20%E5%8A%A0%E9%80%9F%E3%83%95%E3%83%AC%E3%83%BC%E3%83%A0%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%20%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%201%22%20EndSection%20%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22ServerLayout%22%20%E8%AD%98%E5%88%A5%E5%AD%90%20%22Xinerama%20%E3%83%AC%E3%82%A4%E3%82%A2%E3%82%A6%E3%83%88%22%20%E7%94%BB%E9%9D%A2%20%22%E7%94%BB%E9%9D%A20%22%20screen%20%22screen%201%22%20rightOf%20%22screen%200%22%20EndSection%20Section%20%22ServerFlags%22%20Option%20%22Xinerama%22%20%22true%22%20EndSection%20%3C%2FPRE%3E%3CH2%20id%3D%22toc-hId--1182672268%22%20id%3D%22toc-hId--1182672268%22%20id%3D%22toc-hId--260008355%22%3E%3CSPAN%20class%3D%22mw-headline%22%3E%20%E5%AE%9F%E7%B8%BE%20%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%3C%2FP%3E%3CP%3E%E6%AC%A1%E3%81%AE%E5%9B%B3%E3%81%AF%E3%80%81%E4%BB%A5%E5%89%8D%E3%81%AB%E6%A7%8B%E6%88%90%E3%81%97%E3%81%9F%E6%8B%A1%E5%BC%B5%E3%83%87%E3%82%B9%E3%82%AF%E3%83%88%E3%83%83%E3%83%97%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%97%E3%81%A6%E3%81%84%E3%82%8B%20i.MX%2053%20QSB%20%E3%82%92%E7%A4%BA%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3EVGA%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%81%AFFirefox%E3%82%A4%E3%83%B3%E3%82%B9%E3%82%BF%E3%83%B3%E3%82%B9%E3%81%A7%E3%80%81SEIKO%E3%81%AELCD%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%AFcalc%E3%82%A4%E3%83%B3%E3%82%B9%E3%82%BF%E3%83%B3%E3%82%B9%E3%81%A7%E8%A6%8B%E3%82%8B%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22IMX53QSBUbuntuDualDisplayExample.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22IMX53QSBUbuntuDualDisplayExample.jpg%22%20style%3D%22width%3A%20800px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F37778i54B3794E347095A5%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22IMX53QSBUbuntuDualDisplayExample.jpg%22%20alt%3D%22IMX53QSBUbuntuDualDisplayExample.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EIMX53QSBUbuntuDualDisplayExample.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22mce_paste_marker%22%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1115111%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3Ei.MX53%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1115112%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20i.MX53%20QSB%20Ubuntu%20Dual%20Display%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1115112%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHi%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3Ei.mx6q%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AE%E3%83%87%E3%83%A5%E3%82%A2%E3%83%AB%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%A7ubuntu%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%9F%E3%81%84%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%81%9D%E3%81%97%E3%81%A6%E3%80%81LVDS%E3%82%92%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%A8%E3%81%97%E3%81%A6%E4%BD%BF%E7%94%A8%E3%81%97%E3%80%81HDMI%E3%82%922%E7%95%AA%E7%9B%AE%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%A8%E3%81%97%E3%81%A6%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%82%82%E3%81%AE%E3%81%AF%E4%BD%95%E3%81%A7%E3%81%99%E3%81%8B%E3%80%82%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E7%A7%81%E3%81%AEu-boot%E3%81%AE%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%83%91%E3%83%A9%E3%83%A1%E3%83%BC%E3%82%BF%E3%81%AF%E6%AC%A1%E3%81%AE%E3%81%A8%E3%81%8A%E3%82%8A%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3Evideo%3Dmxcfb0%3Adev%3Dldb%2CLDB-XGA%2Cif%3DRGB666%20video%3Dmxcfb1%3Adev%3Dhdmi%2C1920x1080M%4060%2Cif%3DRGB24%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%81%9D%E3%81%97%E3%81%A6%E3%80%81%E7%A7%81%E3%81%AEx%E3%82%A6%E3%82%A3%E3%83%B3%E3%83%89%E3%82%A6%E8%A8%AD%E5%AE%9A%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%81%AF%E6%AC%A1%E3%81%AE%E3%81%A8%E3%81%8A%E3%82%8A%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22InputDevice%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8C%E6%B1%8E%E7%94%A8%E3%82%AD%E3%83%BC%E3%83%9C%E3%83%BC%E3%83%89%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%20%22kbd%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22XkbRules%22%20%22xorg%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22XkbModel%22%20%22pc105%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22XkbLayout%22%20%22us%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22InputDevice%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CConfigured%20Mouse%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%E3%80%8C%E3%83%9E%E3%82%A6%E3%82%B9%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22CorePointer%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%80%8C%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%80%8D%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CLVDS%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%E3%80%8Cvivante%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22fbdev%22%20%22%2Fdev%2Ffb0%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22vivante_fbdev%22%20%22%2Fdev%2Ffb0%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22HWcursor%22%20%22false%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%80%8C%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%80%8D%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CHDMI%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%20%22fbdev%22%20%2F%2F%2F%2F%2F%2F%2F%2F%2F%2F%2F%2F%2F%2F%2F%20%22vivante%22%20%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81X%20%E3%82%A6%E3%82%A3%E3%83%B3%E3%83%89%E3%82%A6%E3%81%AE%E8%B5%B7%E5%8B%95%E3%81%8C%E5%A4%B1%E6%95%97%E3%81%97%E3%80%81%22vivante%22%20%E3%81%8C%202%20%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%82%92%E3%82%B5%E3%83%9D%E3%83%BC%E3%83%88%E3%81%97%E3%81%A6%E3%81%84%E3%81%AA%E3%81%84%E3%82%88%E3%81%86%E3%81%A7%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%20%22fbdev%22%20%22%2Fdev%2Ffb2%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%E3%80%8C%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CLVDS%20%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%E3%80%8C%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CHDMI%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%E3%80%8C%E7%94%BB%E9%9D%A2%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CLVDS%20Screen%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8CLVDS%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%80%8CLVDS%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%E3%80%8C%E7%94%BB%E9%9D%A2%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CHDMI%E3%82%B9%E3%82%AF%E3%83%AA%E3%83%BC%E3%83%B3%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8CHDMI%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%80%8CHDMI%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%20%22ServerLayout%22%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%AD%98%E5%88%A5%E5%AD%90%E3%80%8CDual%20Layout%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E7%94%BB%E9%9D%A20%E3%80%8CLVDS%E7%94%BB%E9%9D%A2%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E7%94%BB%E9%9D%A2%201%20%E3%80%8CHDMI%20%E7%94%BB%E9%9D%A2%E3%80%8D%E5%8F%B3%E3%81%AE%E3%80%8CLVDS%20%E7%94%BB%E9%9D%A2%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%AA%E3%83%97%E3%82%B7%E3%83%A7%E3%83%B3%E3%80%8CXinerama%E3%80%8D%E3%80%8C%E3%82%AA%E3%83%B3%E3%80%8D%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%89%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%81%9D%E3%81%AE%E5%BE%8C%E3%80%812%E3%81%A4%E3%81%AE%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%8C%E6%A9%9F%E8%83%BD%E3%81%97%E3%81%BE%E3%81%97%E3%81%9F%E3%81%8C%E3%80%81%E4%BD%95%E3%81%8B%E3%81%8C%E9%96%93%E9%81%95%E3%81%A3%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3EHDMI%E3%83%87%E3%82%A3%E3%82%B9%E3%83%97%E3%83%AC%E3%82%A4%E3%81%AE%E5%B7%A6%E5%81%B4%E3%81%AB%E3%81%AF%E3%80%81lvds%E3%81%AE%E3%82%B3%E3%83%94%E3%83%BC%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E8%A8%AD%E5%AE%9A%E3%81%8C%E9%96%93%E9%81%95%E3%81%A3%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3CP%20style%3D%22font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%E3%81%93%E3%82%8C%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E7%9F%A5%E3%81%A3%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E7%94%B3%E3%81%97%E4%B8%8A%E3%81%92%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22LVDS.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22LVDS.jpg%22%20style%3D%22width%3A%20640px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F40679iDA69A8CD6C8BA66A%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22LVDS.jpg%22%20alt%3D%22LVDS.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3ELVDS.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22HDMI.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22HDMI.jpg%22%20style%3D%22width%3A%20640px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F40667i11A0716700DB22C7%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22HDMI.jpg%22%20alt%3D%22HDMI.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EHDMI.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E
評価なし
バージョン履歴
最終更新日:
‎09-10-2020 02:27 AM
更新者: