P2040/P2041 Local Bus Specific FAQs

Document created by Omar Cruz Employee on Aug 6, 2012
Version 1Show Document
  • View in full screen mode

Can you please give more details about 32 address signals for the eLBC implementation on P2040?

Below is a detailed explanation of 32 address signals for the eLBC implementation on P2040:

LAD[0:15] - these are multiplexed address/data signals that need to be externally latched using the LALE signal.

LA[16:31] - these are dedicated address signals.

LAD[0] is the most significant address signal and LA[31] is the least significant address signal.


Can the Local Bus FCM support two, 2GByte (16Gbit) NAND devices, if they are the appropriate page size (2K SLC)?

FCM can support two devices, each one is connected to a separate /CS.


Attachments

    Outcomes