P1024/P1015 eSPI/FLASH Specific FAQs

Document created by Omar Cruz Employee on Aug 6, 2012
Version 1Show Document
  • View in full screen mode

Can the P1015 eSPI controller address 4-byte (32-bit) addressable EEPROMs in any situation?

Yes, eSPI controller addresses 4-byte addressable EEPROMs in any situation.


For P1015, is it possible to boot from a 4-byte EEPROM using the on-chip ROM?

No. The software in the on-chip ROM only supports 16-bit addressable or 24-bit addressable EEPROMs.


Attachments

    Outcomes