Even if MTU could be 16K bytes, the average frame could be much smaller. Find out the average frame size and pick up a buffer size that is bit larger than the average frame size. This usually creates a good balance of efficiency between processing time and memory usage. It is much more efficient in terms of processing time to process a frame of 16K in one BD/Buffer of 16K size than in 16 BDs/Buffers of 1K size. However, if all buffers are 16K size while 90% of the frames are 1K, most memory is wasted.
Generally, the ring size should be equal to the number of BD’s required to accommodate the largest possible frame size + 4 extra BDs. However, over here the bandwidth is relatively high (45M) and could be quite bursty. Hence we would suggest starting with "TWO largest possible frame size + 4 extra BDs"
For TX BD ring, (after configured) QE will periodically poll the ring and process the BD that is not empty and then move to next BD. When a BD is actually transmitted, a "transmission complete" event (and interrupt if enabled) will be generated, so the BD/Buffer can be released.
For RX BD ring, (after configured) QE will pre-fetch a BD and then process the BD when data is received. When a packet (frame) is received, a "received" event (and interrupt if enabled) will be generated, so the BD/Buffer can be released/processed. If no empty BD is available during the pre-fetch, an "out-of-BD" error will be reported.
Yes, it should be configured by GUMR[RTSM].