Transferring File Over Serial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transferring File Over Serial

Transferring File Over Serial

For more information verify the U-Boot Manual[1].

You need the "lrzsz" package to add support on minicom to transfer over serial:

aptitude install lrzsz 

Open Minicom and power-on the board. When the U-Boot prompt appears:

=> 

Type the command to transfer the u-boot.bin binary:

=> loady 

Then press the combination keys:

Ctrl+a s 

Then select the option:

ymodem 

A text mode "file explorer" will appear. Select the desired binary (u-boot.bin) pressing "Space" key.

The file transfer will start.

To execute the uploaded file just issue:

=> go 0x100000 

Replace 0x100000 with your TEXT_BASE address.


No ratings
Version history
Last update:
‎09-10-2020 01:37 AM
Updated by: