Wireless and Connected Home of the Future

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless and Connected Home of the Future

Wireless and Connected Home of the Future

Internet of Things nodes are using a wide plethora of heterogeneous wireless connectivity protocols such as: IEEE® 802.15.4, Thread, ZigBee®, 6LoWPAN/IPv6, and BLE. By attending this session you will learn which wireless communication protocol is the right solution for their application requirements, while comparing various communication protocols for 2.4 GHz and sub-1 GHz technologies. This session will provide an overview on commonly used wireless technologies and standards for smart homes and which Freescale microcontroller families are best suited for connected appliance, sensor device or hub product idea.

Presented by Antonio Concio

Presented at DwF Istanbul/Ankara - May 12/14, 2015

Session ID: EUF-IND-T1462

Attachments
No ratings
Version history
Last update:
‎05-04-2015 12:49 AM
Updated by: