Example XPC567XFKIT PinToggleStationery CW210

File uploaded by David Tosenovjan Employee on Nov 7, 2014Last modified by David Tosenovjan Employee on Feb 7, 2020
Version 6Show Document
  • View in full screen mode

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, second LED by software

* loop, initializes and display notice via UART terminal and then terminal ECHO.

* The example configures the device for maximum performance (OPTIMIZATIONS_ON).

* For XPC567XKIT516 it initializes EBI for mounted external SRAM device.

*

* ------------------------------------------------------------------------------

* Test HW:         XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B

* MCU:             PPC5674FMVYA264

* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A

* Fsys:            264/200/150/60 MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          RAM, internal_FLASH

* EVB connection:  ETPUC0(J24-0) -> USER_LED_8 (J5-8)

*                  ETPUC1(J24-1) -> USER_LED_7 (J5-7)(to see blinking LEDs)

*

********************************************************************************

Outcomes