Example MPC5604B Flash Array Integrity Check - using SSD flash drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5604B Flash Array Integrity Check - using SSD flash drivers

Example MPC5604B Flash Array Integrity Check - using SSD flash drivers

This is simple example of the usage of Flash Array Integrity Check (FAIC) function that is available on all MPC56xx devices.

 

The FAIC reads data from selected and unlocked flash blocks and calculates the MISR signature. User can compare the MISR signature calculated by flash controller (in runtime) with MISR calculated by offline tool (this is done during development, not in runtime) from s-record file. If the MISR is identical, we know that the content of selected flash blocks corresponds to content in s-record file and that there are no ECC errors (single bit or double bit ECC errors).

Labels (1)
Attachments
No ratings
Version history
Last update:
‎10-14-2014 07:19 AM
Updated by: