Example MPC5643L 2b RAM and 2b FLASH ECC error injection CW210

File uploaded by David Tosenovjan Employee on Aug 21, 2014Last modified by David Tosenovjan Employee on Mar 27, 2015
Version 3Show Document
  • View in full screen mode

********************************************************************************

* Detailed Description:

* Purpose of the example is to show how to generate Multi bit ECC error in

* internal SRAM or FLASH (user must choose it in the option at the end of main

* function) and how to handle this error with respect to constraints given by

* MPC5643L architecture (ECSM/RGM/FCCU relation and ECC error handling through

* reset). The example is only possible to run in internal_FLASH target. Power-

* -on-reset is required after downloading the code into MCU's flash. The example

* displays notices in the terminal window (setting specified below). No other

* external connection is required.

* ------------------------------------------------------------------------------

* Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon

* Target :         internal_FLASH

* Fsys:            120 MHz PLL0

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0

* EVB connection:  default

*

********************************************************************************

Outcomes