Embedded Graphics

Document created by Andrei Alexandru Trandafir Employee on Aug 4, 2014Last modified by ebiz_ws_prod on Dec 13, 2017
Version 6Show Document
  • View in full screen mode

The attached archive contains the starting point for developing an OpenVG-based embedded graphics application on the Wandboard.

It contains 2 items:


1) The training presentation:

     These are the support slides for the OpenVG presentation held during the Linux Embedded Challenge workshop.


2) The support application:

     This is a sample application meant to aid in setting up the platform for an OpenVG-based application.

     In order to compile it directly on the Wandboard, you will need the arm-linux-gnueabi-g++ compiler. If it is not already installed on the board, you can obtain it by installing the g++-arm-linux-gnueabi package:

 

     sudo apt-get install g++-arm-linux-gnueabi

 

     Use the provided Makefile to build the application. It provides an example on how to:

  • Set up the platform (using X11) and the EGL objects (context, rendering surface etc.)
  • Create an OpenVG path
  • Create a linear gradient paint
  • Create a pattern paint based on a user-generated image
  • Fill and stroke a path
  • Use transformation matrices to scale, rotate and translate a rendered object

 


 


Original Attachment has been moved to: EmbeddedGraphics_Support.zip

Attachments

    Outcomes