Example XPC5643LKIT PinToggleStationery LSM CW210

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example XPC5643LKIT PinToggleStationery LSM CW210

Example XPC5643LKIT PinToggleStationery LSM CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, second LED by software

* loop, initializes and display notice via UART terminal and then terminal ECHO.

* The example configures the device for maximum performance (OPTIMIZATIONS_ON)

* by initialization of instruction cache and enabling of branch prediction.

* Example suppose MCU is configured for LSM (Lock-step mode).

* Its intention is to offer advanced startup code additional to CW stationery.

*

* ------------------------------------------------------------------------------

* Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon

* Target :         internal_FLASH, RAM

* Fsys:            120 MHz PLL0

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0

* EVB connection:  default

*

********************************************************************************

Labels (1)
Attachments
No ratings
Version history
Last update:
‎07-29-2014 01:26 AM
Updated by: