i.MX6 AUDMUX setting when TX <-> RX swapping.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 AUDMUX setting when TX <-> RX swapping.

Jump to solution
922 Views
satoshishimoda
Senior Contributor I

Hi community,

I havea a question about AUDMUX setting.

I understand the setting when not swapping TX and RX in How should I set i.MX6 AUDMUX_PTCR and AUDMUX_PDCR. .

Then, how about in the case of the attached file?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (1)
0 Kudos
Reply
1 Solution
738 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

connections in attached file are quite ambiguous as in

I.MX6 connection AUDMUX port 7 with SSI3 is internally fixed and

usual connection (device_TXD -> AUD_TXD, AUD_RXD->device_RXD)

does not require TXRXEN switch set.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
739 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

connections in attached file are quite ambiguous as in

I.MX6 connection AUDMUX port 7 with SSI3 is internally fixed and

usual connection (device_TXD -> AUD_TXD, AUD_RXD->device_RXD)

does not require TXRXEN switch set.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply