Winbond SPI Flash support for iMXRT685

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Winbond SPI Flash support for iMXRT685

604件の閲覧回数
satoshikawasaki
Contributor I

Hi

We want to use Winbond QSPI Flash with the iMXRT685. (FlexSPI)

Is the above flash part W25X40CLSNIG compatible for iMXRT685 FlexSPI flashing?

RT685: MIMXRT685SFVKB
SPI-NORFlash:W25X40CLSNIG(Winbond)

Please let us know. Any support on the above query will be really helpful

Thanks and Best Regards,

Satoshi Kawasaki

0 件の賞賛
返信
1 返信

562件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @satoshikawasaki 

 

Thanks a lot for reaching our technical support.

 

Regarding the flash memory part you mentioned, it is not listed on our Secure Provisioning Tool, but if you click on edit button, you may modify some parameters so can have compatibility with it.

Please see the next picture from SPTool:

2023-05-30_14-13-40 SPT MEMORIES SUPPORTED.png

Hope this tool can help you to configure it, otherwise, you may try to use another useful tool from a teammate JayHeng to find the memory you want to use.

 

BR.
Pablo Avalos.

0 件の賞賛
返信