source code for AN12239 not founded !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

source code for AN12239 not founded !

Jump to solution
3,208 Views
rans
Senior Contributor I

Hello,

Does anyone knows where we can find source code which is referenced in AN12239:

https://www.nxp.com/docs/en/nxp/application-notes/AN12239.pdf 

Thank you,

ranran

1 Solution
2,904 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, I double checked it, SDK doesn't include this, you need to download the hyper_ram.zip, which includes the AN in the official website as below:

i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP 

View solution in original post

8 Replies
2,904 Views
rans
Senior Contributor I

Hello,

Is there any idea where is the source code?

It is not founded in the packages which were mentioned above.

Thank you,

ranran

0 Kudos
Reply
2,904 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the AN you post, "the SDK used for the example in the application note is SDK_2.3.1_EVKB-IMXRT1050"

so you can download the SDK instead, the package includes the driver of flexspi, what detailed software you need mentioned in the AN??

0 Kudos
Reply
2,904 Views
rans
Senior Contributor I

Hello Joan,

> what detailed software you need mentioned in the AN??

AN12239 described the example code for hyperRAM. This is what I am look for: hyperRAM example code (which is mentioned in AN)

I find in sdk builder download SDK_2.4.2_EVKB-IMXRT1050 .

In that build in board/<>/flexspi I only see hyperFlash example, not hyperRAM.

Can you please refer how I download older sdk and which path in that sdk contains the hyperRAM example ?

Thank you,

ranran

0 Kudos
Reply
2,905 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, I double checked it, SDK doesn't include this, you need to download the hyper_ram.zip, which includes the AN in the official website as below:

i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP 

2,904 Views
jonver
Contributor II

The demo only includes IAR, would a mcuxpresso example be available?

0 Kudos
Reply
2,904 Views
rans
Senior Contributor I

Thank you very much

0 Kudos
Reply
2,903 Views
rans
Senior Contributor I

Hello Joan,

I have browsed the examples there but did not find the hyperRAM example mentioned in the AN.

Can you please tell me which path do you refer to in that zip file ?

Thank you,

ranran

0 Kudos
Reply