Is there a version of mono built anywhere which can run on the iMXRT proc for an embedded linux application?
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The RT series MCU doesn't have the MMU module, in my opinion, it's too hard to run any Linux applications.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------