mono built for the iMXRT1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mono built for the iMXRT1060

896件の閲覧回数
jautry
Contributor IV

Is there a version of mono built anywhere which can run on the iMXRT proc for an embedded linux application?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

886件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The RT series MCU doesn't have the MMU module, in my opinion, it's too hard to run any Linux applications.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信