I flashed my RT1050-EVK with the Segger J-Link 2.1 firmware as described here: NXP MIMXRT1050-EVK — Zephyr Project Documentation
When I run the Zephyr examples, the J-Link is fine:
When I use MCUXpresso to run the examples though, I get this error:
How do I configure the target?
Thanks,
Nathan
No bother at all, this is the note from Segger:
Hello Nathan,
At this time, our Engineering is tentatively scheduling support for this device to be added sometime toward the end of April. You may subscribe to our J-Link Notification email list to be informed as soon as any new features have been added by visiting: https://www.segger.com/notification/subscribe.php?prodid=7. Have a good day.
Best regards,
Shane Titus
SEGGER Microcontroller
Hi Nathan and Kyle,
I'm sorry for the late notice, but the OpenSDA firmware is now available here:
https://www.segger.com/downloads/jlink/OpenSDA_MIMXRT1050-EVK-Hyperflash
Zephyr build targets for flashing and debugging ('ninja flash' and 'ninja debug' respectively) now work as expected on this board. The board documentation is in the process of being updated:
Maureen
Hi Nathan,
According with the Release Notes of the last MCUXpresso release (Version 10.1.0, Nov 2017), it added support for Environment variables in JLink options:
https://www.nxp.com/docs/en/release-note/MCUXpresso-RN.pdf
Have you ensured that you are using this version?
Additionally, have you ensured that the used examples are supported on MCUXpresso?
In case of the MCUXpresso SDK Builder, it only supports GCC ARM Embedded, IAR Embedded Workbench for ARM and Keil MDK toolchains:
https://mcuxpresso.nxp.com/en/select
The following Community document may be also useful:
https://community.nxp.com/docs/DOC-333073
Hope this will be useful for you.
Best regards!
/Carlos
Thanks for the reply CarlosCasillas.
I have version Version: MCUXpresso IDE v10.1.0 [Build 589] [2017-11-14]
And I just re-downloaded the mcuxpresso build from your link, and I still don't see the project:
I see the files on disk:
Hi Nathan,
I have double checked the compatibility, and MCUXpresso SDK for i.MX RT is now supported on MCUXpresso IDE.
However, you need to drag&drop the ZIP file before importing SDK examples. I have attached a video showing the procedure.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------