imx read chip model 1021 vs 1024

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx read chip model 1021 vs 1024

ソリューションへジャンプ
1,165件の閲覧回数
bp1979
Senior Contributor I

Hi,

Is it possible to determine which chip model is active? We would like to create one binary which runs on both 1021 and 1024 cpu's. I would like to distinguish the chip model in software so that I can customize the board files etc.

 

0 件の賞賛
返信
1 解決策
1,128件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
1)Is it somehow possible to read back the chip model from the chip? I can read back a unique chip is for example. Is there some way to distinguish the chip 'type' or 'model'?
-- Unfortunately, in the RT MCU, it hasn't provided a register or similar thing to indicate the type of the MCU.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,161件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is it possible to determine which chip model is active?
-- To be honest, I'm not very clear with this question, so can you clarify it again?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,155件の閲覧回数
bp1979
Senior Contributor I

@jeremyzhou  I am sorry for not being clear. I mean, is it somehow possible to read back the chip model from the chip? I can read back a unique chip is for example. Is there some way to distinguish the chip 'type' or 'model'? I cant find anything like that in the reference manual

0 件の賞賛
返信
1,129件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
1)Is it somehow possible to read back the chip model from the chip? I can read back a unique chip is for example. Is there some way to distinguish the chip 'type' or 'model'?
-- Unfortunately, in the RT MCU, it hasn't provided a register or similar thing to indicate the type of the MCU.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

0 件の賞賛
返信