Hi,
I was able to debug few sample apps of iMX RT685 with onboard LPC Link as LinkServer debug probe and code downloaded to RAM.
Now I want to test few DSP sample apps, so I programmed latest JLink firmware to onboard LPC Link then it detected as SEGGER JLink probe. But when I try to debug any app, received SIGTRAP.
Below is the version info.
MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11]
Firmware_JLink_LPCXpressoV2_20190404.bin
I verified few other posts related to SIGTRAP, but no one solved my problem. If any one has ideas please share.
Thanks,
Yugandhar
Hello @yugandhar421,
In the following post is explained how to update the onboard LPC-Link. Did you replace the LPC-link image?
Best Regards,
Alexis Andalon
Hello @yugandhar421,
In the following link you can download the user manual of the EVK, could you check the default state of the jumpers and see if them match with your board?
Also, only to confirm the LPC link Firmware is the following one?
Best Regards,
Alexis Andalon