iMX RT685 EVK Debug failed with SIGTRAP when using JLink Firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX RT685 EVK Debug failed with SIGTRAP when using JLink Firmware

1,604 次查看
yugandhar421
Contributor II

Hi,

I was able to debug few sample apps of iMX RT685 with onboard LPC Link as LinkServer debug probe and code downloaded to RAM.

Now I want to test few DSP sample apps, so I programmed latest JLink firmware to onboard LPC Link then it detected as SEGGER JLink probe. But when I try to debug any app, received SIGTRAP.

 

Below is the version info.

MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11]

Firmware_JLink_LPCXpressoV2_20190404.bin

 

I verified few other posts related to SIGTRAP, but no one solved my problem. If any one has ideas please share.

 

Thanks,

Yugandhar

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,591 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @yugandhar421,

In the following post is explained how to update the onboard LPC-Link. Did you replace the LPC-link image?

Best Regards,

Alexis Andalon

0 项奖励
回复

1,589 次查看
yugandhar421
Contributor II

Hello @Alexis_A 

 

Yes, I flashed Firmware_JLink_LPCXpressoV2_20190404.bin then it detected as JLink.

0 项奖励
回复

1,567 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @yugandhar421,

In the following link you can download the user manual of the EVK, could you check the default state of the jumpers and see if them match with your board?

Also, only to confirm the LPC link Firmware is the following one?

Alexis_A_0-1623081787502.png

 

Best Regards,

Alexis Andalon

0 项奖励
回复