iMX RT1170-SDIO interface configuration for WiFi module.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1170-SDIO interface configuration for WiFi module.

2,969 Views
Naveed
Contributor II

Hello,

We want to configure iMX RT1170 controller SDIO interface for WiFi module. Can you tell us how to proceed with it. Do you have any example code, it will be helpful if you share it. Also we are doing it on MQX V5 RTOS environment.

Thanks in advance.

0 Kudos
Reply
10 Replies

2,950 Views
Naveed
Contributor II

Thankyou for your reply.

As I have seen the NXP based WiFi modules are there which support for iMXRT boards. We are using iMXRT1170 EVK with LWB5+ series wireless module for WiFi application over SDIO interface.

1. Will iMXRT1170 supports WiFi modules other than NXP? if yes, what changes we have to do in the code?

2. What are the NXP based WiFi-modules supported by iMXRT1170?

 

Thanks in advance.

0 Kudos
Reply

2,961 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
This getting started Guide might be helpful: Getting Started with NXP Wi-Fi® Modules Using i.MX RT Platform | NXP Semiconductors 
This guide contains all the relevant information to interface wireless modules.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

2,949 Views
Naveed
Contributor II

Thankyou for your reply.

As I have seen the NXP based WiFi modules are there which support for iMXRT boards. We are using iMXRT1170 EVK with LWB5+ series wireless module for WiFi application over SDIO interface.

1. Will iMXRT1170 supports WiFi modules other than NXP? if yes, what changes we have to do in the code?

2. What are the NXP based WiFi-modules supported by iMXRT1170?

3. How can I get the WiFi Package for iMXRT1170?

 

Thanks in advance.

0 Kudos
Reply

2,938 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

 

1. In theory it can support different WiFi modules as long they are connected with SDIO/UART and RT1170 features comply with the module requirements.
The drivers, examples we provide were designed to be used with our NXP-based modules and we cannot guarantee that modules from any other vendor would behave similarly with our software. Please note that a porting of this kind is difficult to make and it is up to the customer.
My recommendation is to use our supported WiFi modules.

2. In this getting started guide under the table you can find supported modules by RT1170 and where to find them: Getting Started with NXP Wi-Fi® Modules Using i.MX RT Platform | NXP Semiconductors

3. You can download it from the SDK: Welcome | MCUXpresso SDK Builder (nxp.com)

If you have more questions do not hesitate to ask me.
Best regards,
Omar

2,898 Views
Naveed
Contributor II

Thankyou for your reply,

Any update on this,

Do NXP example code of iMXRT1170 can support WPA_EAP Wi-Fi connection or W-Fi Enterprise connection?

Thanks in advance.

0 Kudos
Reply

2,872 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

As of now the current SDK does not have support for the WPA Enterprise , still, will you be looking for a

an embedded supplicant, or a host-based supplicant?

 

Regards,

0 Kudos
Reply

2,847 Views
Naveed
Contributor II

Hello,

We are looking for embedded supplicant.

Thanks in advance.

0 Kudos
Reply

2,778 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

 

Please help me check the message sent directly, I requested some other information that I understand that might not be public .

 

Regards,

0 Kudos
Reply

2,884 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

I´m sorry for my delayed reply. 
I´m in progress of confirming if this is possible. 
I will answer you as soon as possible.

Best regards,
Omar

0 Kudos
Reply

2,922 Views
Naveed
Contributor II

Thankyou for your reply,

Do NXP example code of iMXRT1170 can support WPA_EAP Wi-Fi connection or W-Fi Enterprise connection?

Thanks in advance.

0 Kudos
Reply