i.mx RT 1175 SDRAM J-Link Boot Scripts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx RT 1175 SDRAM J-Link Boot Scripts

Jump to solution
370 Views
MichaelC_Future
Contributor II

Having issue with connecting/interfacing J-Link to i.MX RT 1175 M7 core using SDRAM. Seen a post with M4 code but not M7. From everything seen on NXP's documentation, M7 boots first. Running an SDK example on SDRAM will fail on the eval board when using a J-link or PE Micro programmer.  However, the same program runs fine on the eval board when using the built in LS programmer.  If it is an SDK example that runs off internal memory, then all three programmers work fine.

0 Kudos
Reply
1 Solution
320 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Please refer to this post to enable debugging on SDRAM: Solved: RT1170 debugging when application is built for SDRAM - NXP Community 

Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
321 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Please refer to this post to enable debugging on SDRAM: Solved: RT1170 debugging when application is built for SDRAM - NXP Community 

Best regards,
Omar

0 Kudos
Reply