Having issue with connecting/interfacing J-Link to i.MX RT 1175 M7 core using SDRAM. Seen a post with M4 code but not M7. From everything seen on NXP's documentation, M7 boots first. Running an SDK example on SDRAM will fail on the eval board when using a J-link or PE Micro programmer. However, the same program runs fine on the eval board when using the built in LS programmer. If it is an SDK example that runs off internal memory, then all three programmers work fine.
Solved! Go to Solution.
Hello
Please refer to this post to enable debugging on SDRAM: Solved: RT1170 debugging when application is built for SDRAM - NXP Community
Best regards,
Omar
Hello
Please refer to this post to enable debugging on SDRAM: Solved: RT1170 debugging when application is built for SDRAM - NXP Community
Best regards,
Omar