i.MXRT117x - Can FlexSPI1 and FlexSPI2 both be run at full clock speed of 133MHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT117x - Can FlexSPI1 and FlexSPI2 both be run at full clock speed of 133MHz?

1,062 Views
KMurp
Contributor III

We are trying to run 2 QSPI NOR Flash devices, one on FlexSPI1 as XIP and the second on FlexSPI2 for data logging.

Pins for FlexSPI1 are GPIO_SD_B2_06 through 11 with GPIO_SD_B2_05 left floating for DQS.

Pins for FlexSPI2 are GPIO_EMC_B2_10 through 16, with GPIO_EMC_B2_12 left floating for DQS.

Everything works, however, we can't get FlexSPI2 to run at full clock speed of 133MHz.  If this is possible, we haven't figured out how to do it.  We can only run FlexSPI2 at half clock frequency.  The DQS pin on GPIO_EMC_B2_12 doesn't seem to matter if it's configured as the DQS or not.

Is it possible to run FlexSPI2 at full clock frequency, and how should we configure that?

Thanks,

Kevin

0 Kudos
Reply
4 Replies

1,026 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @KMurp ,

Yes, flexspi2 can run at 133Mhz. Have you configureflexspi2 DQS to kFLEXSPI_ReadSampleClkLoopbackFromDqsPad?

 

Regards,

Jing

0 Kudos
Reply

1,014 Views
KMurp
Contributor III

Thank you for the quick reply!

Yes, we tried that and could not get full clock speed.  Any other suggestions would be appreciated.

 

Kevin

0 Kudos
Reply

998 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @KMurp ,

Did you follow the flexspi hardware design rule in RT1170 hardware design guide?

 

Regards,

Jing

0 Kudos
Reply

961 Views
KMurp
Contributor III

Yes.  I went back to the Hardware Design Guide and verified that our design is consistent with the rules in the latest document.

Thanks,

Kevin

0 Kudos
Reply