I want use the i.MX RT1050 with an external 8/16-bit SDRAM and an external 8/16-bit SCL NAND flash.
Are there some schematics to follow as reference?
Thanks in advance.
Angelo
Solved! Go to Solution.
For this issue, refers to IMXRT1050 reference manual, chapter 48.4.3.
Best regards,
Angelo
You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)
Hi Angelo,
In case of the SRAM implementation, you could refer to the i.MX RT1050 EVK. On the following link you could find the “i.MXRT1050 EVK Extended Feature Example Code and HW guide” where board schematics are included:
https://www.nxp.com/webapp/Download?colCode=i.MXRT1050-EX-CODE-AND-HW-GUIDE&appType=license
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Carlos,
thank you for your kindest answer.
I had already checked the archive "i.MXRT1050 EVK Extension Feature Example Code and HW Guide", but I find only info about CSI, FlexIO, FlexSPI, LPSPI, PWM, SPDIF and WiFi. Nothing about the SLC NAND Flash.
Best regards,
Angelo
For this issue, refers to IMXRT1050 reference manual, chapter 48.4.3.
Best regards,
Angelo