Hi
I watched this thread https://community.nxp.com/t5/i-MX-RT/IMXRT1064-Power-Up-sequence/m-p/994938/thread-id/5905 .
And I have more question.
If I don't have a backup battery then the processor can connect all power at same time?
If it is yes, I can using only one LDO or converter without on-chip DCDC?
Allen
解決済! 解決策の投稿を見る。
Hello,
Yes. It is correct.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hello,
Yes, if the lowest sleep power mode(SNVS Mode) is not necessary in your app, SNVS_IN can be POR together with other power domain to implement true one LDO or DC-DC regulator in system.
Hope it help you. Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi fangfang
Thanks for your reply.
I referenced the "IMXRT1064CEC.pdf".
In chapter 4.1.1 Table.7 Absolute maximum ratings, I saw VDD_SOC_IN max 1.6V.
To simplify the power supply.
I think there are 2 way to achieve. Am I right?
1. one LDO-3.3V and using on chip DCDC conveter
2. one LDO-3.3V and one LDO-1.1V
I'm first using this type processor.
I was using simple MCU before.
Thanks for your patience.
Allen
Hello,
I think there are 2 way to achieve. Am I right?
1. one LDO-3.3V and using on chip DCDC conveter
2. one LDO-3.3V and one LDO-1.1V.
For the RT application, Don't use one LDO-1.1V. Because VDD_SOC_IN is "Core supplies input voltage" .You may refer to the design for the EVK.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi fangfang
Thanks for your reply.
For the RT application, Don't use one LDO-1.1V. Because VDD_SOC_IN is "Core supplies input voltage" .You may refer to the design for the EVK.
So I can using LDO-3.3V supply all processor power except VDD_SOC_IN.
And VDD_SOC_IN use internal DCDC to supply.
Is my understanding correct?
Allen
Hello,
Yes. It is correct.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------