i.MX RT 1064 EVK audio example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT 1064 EVK audio example

Jump to solution
2,304 Views
radhikakrishnan
Contributor III

Hello,

I have an i.MX RT 1064 and I have installed the MCUXpress SDK with FreeRTOS feature.

The helloworld example is working fine.

I need to verify the audio output of the EVK and ethernet functionalities - in FreeRTOS.

I tried the examples for audio - evkmimxrt1064_dev_audio_generator_freertos, evkmimxrt1064_dev_audio_speaker_lite_bm, evkmimxrt1064_dev_audio_generator_lite_bm, evkmimxrt1064_dev_audio_speaker_bm, evkmimxrt1064_dev_audio_generator_bm. But none of these gives any audio output on the head phone connected to the audio jack. I tried debugging and enabled the macro - USB_DEVICE_CONFIG_USE_TASK to 1U, but still no result and no error.

Can you please let me know if I am going in the right direction? 

thanks,

Radhika

Tags (1)
0 Kudos
Reply
1 Solution
2,068 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Radhika Krishnan,

   Thank you for your updated information.

   Do you check the readme.pdf in the project? That readme tell you the detail project information.

   Take the MIMXRT1064-EVK board as an example. J9 usb port is the audio port after you download the code to the RT chip.

   This is my test result:

pastedImage_1.png

When you plug the J9 to your PC, you will find that USB is the audio port.

More details, please check the readme.pdf.

Wish it helps you!
Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
2,068 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Radhika Krishnan ,

  Please tell me which SDK version you are using?

   Do you use the following project?

pastedImage_1.png

If you are not using the SDK2.6.0, please download the newest SDK from this link:

Welcome | MCUXpresso SDK Builder 

and try it again.

If you still have questions about it, please kindly let me know, I will help you to check it.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,068 Views
radhikakrishnan
Contributor III

Hello Kerry,

I am using SDK version 2.6.0 and the project is same as you showed.

Is the project expecting a USB microphone input? I could not understand which audio source is being used to play in the speaker. 

regards,

Radhika.

0 Kudos
Reply
2,069 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Radhika Krishnan,

   Thank you for your updated information.

   Do you check the readme.pdf in the project? That readme tell you the detail project information.

   Take the MIMXRT1064-EVK board as an example. J9 usb port is the audio port after you download the code to the RT chip.

   This is my test result:

pastedImage_1.png

When you plug the J9 to your PC, you will find that USB is the audio port.

More details, please check the readme.pdf.

Wish it helps you!
Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,068 Views
radhikakrishnan
Contributor III

Thank you, kerryzhou

It worked.

Is there any examples to use the ethernet port of the IMX RT1064 EVK?

regards,

Radhika.

0 Kudos
Reply
2,068 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Radhika,

  Please check SDK_2.6.0_EVK-MIMXRT1064\boards\evkmimxrt1064\driver_examples\enet

  Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,068 Views
radhikakrishnan
Contributor III

Thank you.

0 Kudos
Reply