Hi
I am considering to do prototype development using i.MX RT1010 EVK with Zephyr OS but as I see there is some discrepancy in documentation. On NXP docs I see that it is supported by Zephyr OS but I don't see it in the list of supported boards on zephyr wiki. Do I need to port board packages to i.MXRT1010 or will it be supported officially ?
Please advise.
I was able to build MicroPython based Zephyr OS for iMX RT on Linux but I have not be able to flash test it due to JTAG winding up.
I might give another try this weekend
God blesses!!!
Best regards,
Sanyaade
Hi Andrii:
As far as I know, the most up-to-date list is at
Supported Boards — Zephyr Project Documentation
This page gets regenerated rightly based on the latest source
From that I can see that the following RT boards are supported
Regards
Daniel
Hi Andrii,
Yes, RT1010 will be supported. There is a pull request available that we hope to get merged after the Zephyr 2.1 release. Currently the master branch is closed to new features to prepare the release, and will reopen after the release is complete. In the meantime, you can use the pull request branch.
Enable imxrt1010 by jhqian · Pull Request #19335 · zephyrproject-rtos/zephyr · GitHub
Maureen
Hi Maureen,
similarly the product page mentions mbed support: will that be provided in the future as well ?
Regards,
MM
Yes
Hi
Question is will i.MX RT1010 be supported if yes then when ?
--
Regards,
Andrey Loginov | Solution Architect | ARMA Instruments AG | https://armainstruments.com<https://armainstruments.com/>;
T: +41449746005