Hi,
Board = imxrt1064evk.
SDK = SDK_2.7.0_EVK-MIMXRT1064
I am trying to port ew_gui(ew_gui_bezier_clock) to free rtos.
I am getting error ew_gui ew_bsp_clock.c used systick handler and free rtos also using systick handler.
If i comment systick handler in ew_bsp_clock.c there is no error but only idle thread is running GuiThread(priority 5) is not running.
How to solve this issue ?
How to port ew_gui to free rtos ?
Thanks & Regards
Vasu
解決済! 解決策の投稿を見る。
Hi,
I can able to port ew_gui demo to free rtos.
I have another issue multitasking is not working.
ew_gui ported to tcp_echo_free_rtos project if i run only tcp thread running fine and only ew_gui thread running fine.
If i run both threads only ew_gui running other threads not running.
How to solve this issue ?
Thanks & Regards
Vasu
Hello Vasu,
Have you tried increasing the heap size of the project?
Regards,
Victor
Hi Victor,
I found the problem.
Thanks & Regards
Vasu
Hi Victor,
Thank you for your reply,
Heap size already increased but still same issue.
If i run ew_gui thread other network threads(mqtt,http) not running ethernet led(see IMG_20200203_091644) also not blinking and adc thread running with wrong value.
If i commend ew_gui threads other thread running fine mqtt,http server, etc..
Please give some suggestion.
Default ram - SRAM_0C size - 0xc0000
disabled cache :
SCB_DisableDCache();
SCB_DisableICache();
Debug log :
Initializing PHY...
************************************************
1.00.00.00
************************************************
IPv4 Address : 192.168.6.212
IPv4 Subnet mask : 255.255.255.255
IPv4 Gateway : 192.168.6.300
************************************************
Queue Creation Success
Create UI thread... Initialize Realtime Clock... [OK]
Initialize Display... [OK]
Initialize Touch Driver... [OK]
Initialize Memory Manager... [OK]
Initialize Graphics Engine... [OK]
Create Embedded Wizard Root Object... [OK]
Create Embedded Wizard Viewport... [OK]
---------------------------------------------
Target system IMXRT1064-EVK
Color format RGB565
MemoryPool address 0x8107F800
MemoryPool size 16254976 bytes
Framebuffer address 0x81000000
Doublebuffer address 0x8103FC00
Framebuffer size 480 x 272
EwScreeenSize 480 x 272
Graphics accelerator PXP
Vector graphics support enabled
Warp function support enabled
Index8 bitmap resource format enabled
RGB565 bitmap resource format enabled
Bidirectional text support enabled
Operating system FreeRTOS
External flash device none
Toolchain GCC
C-Compiler version 8.3.1
Build date and time Jan 31 2020, 17:09:16
Runtime Environment (RTE) version 9.20
Graphics Engine (GFX) version 9.20
Max surface cache size 2097152 bytes
Glyph cache size 256 x 256
Max issue tasks 100
Surface rotation 0
---------------------------------------------
Connecting to MQTT broker at 192.168.6.214...
Thanks & Regards,
Vasu