Hello,
I am working very hard by the eDMA transfer between peripheral (ADC_ETC) and memory application.
I have the need to buffer the (ADC result) via eDMA to the memory with very high resolution.
It is quite hard to learn the eDMA application only due to the reference manual. The SDK v2.11.0 only provide example code for the memory to memory transfering, but no peripheral to memory.
Can anyone provide a application note or example code just for better understanding how the eDMA work with peripheral together?
many thanks
best regards
Hi @auftrag2021 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can anyone provide an application note or example code just for a better understanding of how the DMA works with peripheral together?
-- To provide the fastest possible support, I'd highly recommend you to refer to the post, these tutorials also suit the i. MX RT.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------