Yocto support for iMXRT1180 Crossover MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto support for iMXRT1180 Crossover MCU

跳至解决方案
825 次查看
vilas_shetty
Contributor III

Hello

I am trying to find out whether iMXRT1182 processor will support yocto Linux. I am developing a project which requires OS support. Can anyone help me out in this. How can i get started with iMXRT1182 MCU.

 

 

0 项奖励
回复
1 解答
771 次查看
samsaprunoff
Contributor V

Good day,

The RT processors support a number of OS's:

- Zephyr  (which was created/modelled after Linux if I recall)

- FreeRTOS

- uTasker

- Nuttx (https://nuttx.apache.org/)

There are probably others, but these are a few that come to mind. 

Cheers,

Sam

 

 

 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
752 次查看
vilas_shetty
Contributor III

Thank you Pavel Hernandez and samsaprunoff 

 

800 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, however the RT1180 is a Cross MCU and does not have support for OS, if you want to use a Linux system, I recommend review the IMX6 or IMX8.

i.MX 8 Series Applications Processors | Arm® Cortex®-A72/A53/A35/M4 cores | NXP Semiconductors

i.MX 6 Series Applications Processors | Multicore Arm Cortex-A7/A9/M4 | NXP Semiconductors

Best regards,
Pavel

0 项奖励
回复
791 次查看
vilas_shetty
Contributor III
Hello Pavel Hernandez, Thank you for your response.
Well it means i wont be able to have any os into iMXRT series of MCU. Then how these MCU's are setup. it it only with bare metal or it can support RTOS too?
0 项奖励
回复
772 次查看
samsaprunoff
Contributor V

Good day,

The RT processors support a number of OS's:

- Zephyr  (which was created/modelled after Linux if I recall)

- FreeRTOS

- uTasker

- Nuttx (https://nuttx.apache.org/)

There are probably others, but these are a few that come to mind. 

Cheers,

Sam

 

 

 

0 项奖励
回复
779 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, yes this can be programed as bare metal or using the HAL library from NXP available on the examples SDK and yes is compatible with RTOS.

Best regards,
Pavel

0 项奖励
回复