Good day
I am debugging an RT1176 processor with NXP's MCU-Link Debug Probe. I would like to obtain detailed information about the interrupts in my project, so I tried to configure the project for SWO Tracing.
These are the steps I followed:
To verify my SWO Tracing setup, I followed the above steps on the eaimxrt1176_cm7 Embedded Artist SDK example project. Note that one must enable the Pins tool for the project before the changes to the pins can be made (because it is an SDK project).
According to the project's main(), the PIT interrupt should occur once per second:
However, the trace shows that it only occurs about once every 7s (see "measured interval"):
The Cortex M7 core root clock is set to 996MHz. It seems like the SWO tracing is using the core root clock to determine the interrupt timing, instead of the CSTRACE clock. This could explain the multiplier of approximately 7, since 996/132 = 7.54.
I have the same problem in both MCUXpresso v11.5.1 and MCUXpresso v11.6.0.
Is this a bug in the SWO Tracing of the RT1176? Is there a known fix?
Thanks in advance.
已解决! 转到解答。
Good day @Pavel_Hernandez
Thanks for the help.
This problem is solved in MCUXpresso IDE v11.6.1, as stated in the release notes.
Regards
D_TTSA
Good day @Pavel_Hernandez
Thanks for the help.
This problem is solved in MCUXpresso IDE v11.6.1, as stated in the release notes.
Regards
D_TTSA
Hello,
I'm still following your case, I'm working to get a solution to this issue. When I have more comments I will contact you, my I apologize for the inconvenience this may cause.
Best regards,
Pavel
Hello,
I talked to the IDE department and they reproduced the same issue they will work on a solution for the next release, unfortunately, we do not have a date for this release, I apologize for the inconvenience this may cause.
Best regards,
Pavel
Okay, thank you for the update.
So it is an IDE problem then? So we can expect that the MCUXpresso IDE version after v11.6 will include a fix for this?
Would it be possible for you to post in this thread once the fixed MCUXpresso IDE version has been released?
D_TTSA
Hello,
Unfortunately, there is not much information about your specific issue but I find this information maybe could help you, if not please let me know.
How to Enable SWO Trace for i.MX RT10xx Series (nxp.com)
Best regards,
Pavel
Update @Pavel_Hernandez
I found this document (attached), which has been recently updated to include a section on how to configure the RT1176 for SWO tracing.
By following these steps exactly, I get the incorrect interrupt timing information (as described in my first post).
Please get back to me as soon as you can.
D_TTSA
Update @Pavel_Hernandez @jingpan @kerryzhou
I tested out my earlier hypothesis as to why there is a timing problem.
In the eaimxrt1176_pit_cm7 example, I decreased the M7's clock frequency to 264MHz (I couldn't decrease it to 132MHz because the required prescaler value is out of bounds). I left the CSTRACE clock frequency at 132MHz. I clicked "Update Code" in ConfigTools.
I decreased the timer period to 1s:
Then I ran the debug again, and again set the SWO config clock speed to 132MHz.
Now the 1s interrupts occur every 1s 999ms - proving that M7_cloc_freq / CSTRACE_clock_freq is the factor that is unaccounted for in the SWO trace's time calculations.
I have uploaded my project too, so that NXP can download it and try it out for themselves.
Please could NXP get back to me on this with a fix or work-around, as soon as possible.
Hello,
I appreciate all your information, I will check your information and when I have more details I will contact you. I apologize for the time long this maybe will take.
Edit: Let me get in these days an RT1170 to reproduce this issue. Here are other notes in other threads for SWO RT1170.
[SWO with NXP i.MX RT1064-EVK Board - NXP Community] [MCUXpresso IDE SWO Trace Guide (nxp.com)] [How using SWO on RT1170 and MIMXRT1170-EVK board ? - NXP Community] in the 3rd thread review the response from Kerry, maybe could help you.
Best regards,
Pavel
Thanks for the threads. I have read them, and unfortunately they do not address my issue.
So far, I have been working with the MCU-Link external debugger, my employer's own PCB and JTAG connection, and Embedded Artists' RT1176 uCOM board.
However, I have just reproduced the problem on NXP's RT1170-EVK, with the evkmimxrt1170_pit_cm7 SDK example (SDK version 2.12.0).
Follow my steps below:
The SDK example configures these interrupts to occur once per second (1s period), so there is clearly something wrong with the SWO tracing.
The fact that I could reproduce this problem on the RT1170-EVK with its onboard debugger proves that the MCU-Link Debug probe is not the cause of the problem. It also proves that it is not to do with Embedded Artists' RT1176 uCOM board. This allows NXP to debug this internally.
@Pavel_Hernandez If you follow the above steps, you will be able to recreate my problem on an RT1170-EVK.
Please let me know if you have any further information.
D_TTSA.
To further specify the cause of the problem, I followed the above steps, but using the evkmimxrt1170_pit_cm4 SDK example (also using SDK version 2.12.0, RT1170-EVK and its internal debugger with LPC-LINK2 firmware).
Now, the SWO tracing is performed on the Cortex-M4 core.
See the result below:
Now the interrupts measure as 2s 975ms apart instead of 1s apart.
This brings me back to one of my first few posts in this thread. I said that I believed that the factor offset is the traced processor core's root clock frequency divided by the CSTRACE clock frequency.
In the evkmimxrt1170_pit_cm4 example,
the Cortex-M4's root clock frequency = 4320/11 = 392.7272...MHz:
The CSTRACE clock frequency is still 132MHz.
Therefore, the time factor that is shown in the SWO tracing is:
This confirms that my above hypothesis is true - the timing error factor is equal to the traced processor core's root clock frequency divided by the CSTRACE clock frequency.
This also shows that the problem is not specific to the Cortex-M7 core.
I believe it is a problem with the MCUXpresso IDE's SWO tracing software for the RT1176.
Please follow up with the relevant NXP team and get back to me on this.
D_TTSA
Please note that you can also reproduce this by running either the evkmimxrt1170_pit_cm7 project or the evkmimxrt1170_pit_cm4 project on the RT1170-EVK.
Please get back to me as soon as possible regarding this, because I need this feature to debug my own project.
D_TTSA