Which HW_OCOTP_TIMINGs are correct?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which HW_OCOTP_TIMINGs are correct?

1,223 Views
caseydavis
Contributor IV

The RT1050 sec ref manual has the following guideline for HW_OCOTP_TIMINGs (section 8.3.3):

tRELAX = tHP_PG = (HW_OCOTP_TIMING[RELAX]+1)/ipg_frequency > 16.2ns

And the RT1060 ref manual has:

tRELAX = tHP_PG = (HW_OCOTP_TIMING[RELAX]+1)/ipg_frequency > 100ns

Which should I observe?

Tags (1)
0 Kudos
Reply
3 Replies

1,126 Views
carstengroen
Senior Contributor II

Some (maybe useful) related info here: https://community.nxp.com/thread/492451 

0 Kudos
Reply

1,125 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The RT1060's information  are right. And the updated RT1050 RM are fixed the information.Please find the detail information as it. https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true . Thanks for your feedback.

Best regards.

0 Kudos
Reply

1,125 Views
caseydavis
Contributor IV

I'm also seeing a discrepancy about how to calculate the condition that the strobe programming timing should meet. The RT1060 ref manual has t_pgm calculated as

t_pgm = [(STROBE_PROG+1) – 2×(RELAX_PROG+1)]/ipg_clk_freq

While the sec ref manual has

t_pgm = [(STROBE_PROG+1) – 2×(RELAX+1)]/ipg_clk_freq

The difference being RELAX_PROG (from TIMING2 register) vs RELAX.

Which is it?

0 Kudos
Reply