Hello,
in the RT1020 reference manual you can find the following explanations for FlexSPI IP TX/RX watermark levels
Kind regards,
Stefan
解決済! 解決策の投稿を見る。
Hi Stefan,
Sorry for the confusion. Your understanding is correct, if there are more than watermark bits free the DMA request will be triggered. "empty level" does mean how many FIFO entries are free.
Regards,
Victor
Hello Stefan,
What does "DMA request when the filling level is no less than the Watermark level" mean?
When will the DMA request be generated?
In the case of TXWMRK, the DMA request will be triggered when the TX FIFO exceeds the Watermark. For the RXWMRK, the DMA request will be triggered when the RX FIFO exceeds the Watermark level. In both cases, DMA filling has to be enabled.
What is a write window?
I'm checking this with the applications team, I will give you an update as soon as possible.
Regards,
Victor
Hello Victor
thank you for answering and checking with the applications team.
Does exceed for TX mean "if there are less than watermark bits in FIFO trigger DMA request"?
or does it mean "if there are more than watermark bits in FIFO trigger DMA request"?
The second option does not make any sense to me because if I trigger a DMA request every time there are more than tx watermark bits in FIFO I will fill the FIFO more and more until I overrun TX FIFO size.
Kind regards,
Stefan
Hello Stefan,
Does exceed for TX mean "if there are less than watermark bits in FIFO trigger DMA request"?
or does it mean "if there are more than watermark bits in FIFO trigger DMA request"?
It means that if there are more than watermark bits in the FIFO the DMA request will trigger. The DMA trigger request will trigger as soon as the FIFO level exceeds the watermark.
What is a write window?
The write window is total size of TX FIFO Data Register (TFDR0 - TFDR31), or total size of AHB Memory Map for TX FIFO write access.
Regards,
Victor
Hi Victor,
sorry for the late reply.
I am confused by the wording of the Reference Manual because the LPUART defines this
If I set my TXWATER to 2 and there is only one element in FIFO the LPUART will trigger a DMA transfer.
If I use this description for the FlexSPI it will be like if there are 3 elements in FIFO but TXWATER is set to 2 it will trigger a DMA transfer which will fill the FIFO even more -> generates another DMA request because there are still more than 2 elements in the FIFO. This would fill the FIFO until an overrun occurs.
If the FlexSPI is defined as if there are more than watermark bits free the DMA request will be triggered it makes sense for me. Does the FlexSPI "empty level" mean how many FIFO entries are free?
Kind regards,
Stefan
Hi Stefan,
Sorry for the confusion. Your understanding is correct, if there are more than watermark bits free the DMA request will be triggered. "empty level" does mean how many FIFO entries are free.
Regards,
Victor
Thank you!