Unable to debug on IMXRT1050-EVKB (0 available SWD Devices detected).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to debug on IMXRT1050-EVKB (0 available SWD Devices detected).

跳至解决方案
10,761 次查看
Murtn
Contributor II

I'm trying to debug an example project on a IMXRT1050-EVKB using MCUXpresso IDE. I've imported SDK example "evkbimxrt1050_iled_blinky" built it and tried to debug it. 

When starting the debugging I get prompted with a message saying:

SWD Configuration. 0 available SWD Devices detected.

How can I resolve this problem?

Kind regards,

 

 

标签 (1)
0 项奖励
回复
1 解答
10,741 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the attachment for it which is similar with the RT1050.

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

在原帖中查看解决方案

6 回复数
9,532 次查看
expertsleepers
Contributor III

Does anyone actually know how to stop the boards getting into this situation in the first place? Having to constantly use the Boot Utility to recover is not sustainable.

 

0 项奖励
回复
9,751 次查看
ejd037
Contributor I

It would be great if one of the moderators would put recover_rt1064.pdf, and the like, on all Get Started pages for the EVK boards. Took me most of the day to stumble on this. Thanks again to "fangfang" for posting it.

0 项奖励
回复
10,539 次查看
andy4
Contributor I

This worked for the MIXRT1060-EVK board when it had the "0 available SWD Devices" message as well.

10,742 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the attachment for it which is similar with the RT1050.

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

9,456 次查看
bloom11
Contributor II

Thanks, this PDF that you shared, explaining the process to access the recovery mode of the board/MCU work fine on the 1060(tested)/1064(tested)/1062 and maybe 1050 from the different comments i have seen. It has been really useful in my case and save me a lot of time.

0 项奖励
回复
10,735 次查看
Murtn
Contributor II

This seemed to do the trick.

Thank you!

0 项奖励
回复