USB Speaker Can not work in audio class 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Speaker Can not work in audio class 2.0

1,268件の閲覧回数
pollywang
Contributor I
  • Dear NXP Team:

        Now I am working around  USB Audio Speaker Demo for  Audio Class 2.0 driver with RT1021 in windows10 and android System. But I have some confusion.Firstly. I have tried to modify usb device descriptor to meet usb audio class 2.0.  I successfully get enumeration In windows10 and android.I find there is no  data transferred from host to device in Isochronous out endpoint 
    and control interface can send valid control data.  Is there something other needed to modify? 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,104件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Paul,

I just checked on mac OS, audio class 2.0 is OK. So, this is the limiation of windows platform, not SDK issue.

Regards,

Jing

0 件の賞賛
返信