USB Certification Guides

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Certification Guides

Jump to solution
1,445 Views
namsu_mun
Contributor III

Hi,

I'm looking for "USB Certification Guides" for RT1064 EVB, especially need test result of EHSETT.

Thank you,

Namsu

Labels (1)
0 Kudos
Reply
1 Solution
1,431 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, there is no separate USB certification guides for it.. One may refer to the application note for the it.

URL:https://www.nxp.com/docs/en/application-note/AN12409.pdf.

 

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

View solution in original post

1 Reply
1,432 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, there is no separate USB certification guides for it.. One may refer to the application note for the it.

URL:https://www.nxp.com/docs/en/application-note/AN12409.pdf.

 

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------