Hello All,
i am working on IMX RT processor, i am able to enter into SDP mode from Application using ROM API and from selection of BOOT MODE pins. i would like to know, in what other conditions processor can enter into Serial Download mode.
for ex.
1. in case of any SW exception or hard fault, will it enter into serial download mode.
2. in case of any memory corruption while writing into flash, will it enter into serial download mode.
or if there is any other scenario, how it can enter into serial download mode.
Can anyone help me on this.
Thanks & Regards,
Anshul
@jay_heng if the images is signed or signed and encrypted , in that case also will boot rom checks the image validity?
and in-case in above scenarios image is not proper will it enter in SDP mode?
Thanks & Regards,
Anshul
SDP mode is mainly used to upgrade app image. ROM API and BOOT MODE pin are the two main ways to enter this mode
SW exception or hard fault has nothing to do with SDP mode.
memory corruption while writing into flash may cause processor to enter SDP mode, if boot header of app image is destroyed.
In a word. if bootROM cannot find proper image in external memory during boot process, it will switch to SDP mode.