Security binary file for SMT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security binary file for SMT

1,157 Views
kensu
Contributor V

Hi 

I use RT1015 and I had verify my .sb file.

In RD development stage, I use mfgtool to program the sb file to flash.

Now, the sb firmware will be released to SMT factory for mass production.

We need write firmware to Flash and write AES key in production line.

 

My question is how to write sb file to flash with flash programmer tool ex: All-100

 

Regards

Ken

 

0 Kudos
Reply
1 Reply

1,139 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

For production you can use this tool. https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/i-MXRT-Production-tool-RT-Flash-v1-0-0-is-releas...

Hope it helps!

Best regards,

Felipe

0 Kudos
Reply