Hello, all
Customer(Panasonic) wants to reduce the noise on the pin of 「IOMUXC_GPIO_AD_B1_05_CSI_MCLK」by decline the drive strength by following two methods?
1. By setting the appropriate Rdrv impedance value
2 To change the prescaler of CSI_MCLK. The current prescaler is 1/2, and customer wants to change the prescaler to decline the strength of drive.
How about the two method?
Best regars
ZHOU
解決済! 解決策の投稿を見る。
Hi Zhou,
Does the noise here means RE noise? Could you pleae check this with customer?
if yes, i think the first question can be used. But i don't think the second one can reduce RE result.
Hello, @lucas_cao
Does the noise here means RE noise? Could you pleae check this with customer?
→Yes. The customer means RE(radiated emission) . They concerns about the RE of the CSI MCLK. and want to reduce the RE noise.
Currently , they measure the pin of CSI MCLK.
Although the power supply is 3.3 V , the amplitude of the CSI MCLK is about -1.8 V ~~ 5.1V.
Do you have any comments about the big the amplititude of -1.8 V ~~ 5.1V?
Best regards
ZHOU
Reduce the Drive strength values in pad settings will help on this.