RT685 I3C port - pins 2_29, 2_30 - Is IOCON ODENA Open-drain mode enable ignored?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT685 I3C port - pins 2_29, 2_30 - Is IOCON ODENA Open-drain mode enable ignored?

跳至解决方案
1,388 次查看
dash
Contributor II

Pins set to mode 1 (I3C0__SCL, I3C0__SDA).

I do not see a difference whether the IOCON ODENA (Open-drain mode enable) bit is set or not.

I would expect, especially operating in I2C mode, it needs to be open-drain to work.

Thanks,

Dan

0 项奖励
回复
1 解答
1,372 次查看
Dezheng_Tang
NXP Employee
NXP Employee

Hi,

    Bit 10 is the pseudo open drain configuration. This bit has no effect if you use I3C controller pins for I2C communication.

That’s why we mentioned this in our spec.

Dezheng_Tang_0-1653516522749.png

Once you configure I3C_PUR pin, it’s internally pull SDA high. If you don’t use PUR pin, you will need to have external Pull-up on SDA line for I2C communication. Either way, it’s needed when bus is in open drain condition.

More details on the bus conditions, push-pull or open-drain, can be found on MIPI I3C spec. v1.1, section 5.1.3.

 

Tom

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,370 次查看
dash
Contributor II

Thank you.

We are using the port in I2C mode and have a pull-up on the data line.

0 项奖励
回复
1,373 次查看
Dezheng_Tang
NXP Employee
NXP Employee

Hi,

    Bit 10 is the pseudo open drain configuration. This bit has no effect if you use I3C controller pins for I2C communication.

That’s why we mentioned this in our spec.

Dezheng_Tang_0-1653516522749.png

Once you configure I3C_PUR pin, it’s internally pull SDA high. If you don’t use PUR pin, you will need to have external Pull-up on SDA line for I2C communication. Either way, it’s needed when bus is in open drain condition.

More details on the bus conditions, push-pull or open-drain, can be found on MIPI I3C spec. v1.1, section 5.1.3.

 

Tom

 

0 项奖励
回复