RT117x: where is the FORCE_COLD_BOOT fuse reflected?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT117x: where is the FORCE_COLD_BOOT fuse reflected?

跳至解决方案
1,127 次查看
mastupristi
Senior Contributor I

On the Ref Man I read:

Screenshot_2023-04-11_18-15-01.png

the FORCE_COLD_BOOT should be reflected in SRC_SBMR...

I looked for SRC_SBMR and found two registers, but in neither of them do I seem to see the bit reflected by the FORCE_COLD_BOOT fuse.

Could you point me to which register and which bit I find it in?

best regards

Max

标记 (3)
0 项奖励
回复
1 解答
1,104 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

This is true. Confirmed by support engineer.

 

Regards,

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,111 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

For RT1170, I think this fuse bit is not touched by ROM. You can ignore it.

 

Regards,

Jing

0 项奖励
回复
1,107 次查看
mastupristi
Senior Contributor I

I think this fuse bit is not touched by ROM. You can ignore it.

Is this your feeling or do you have written confirmation in some document?
Because the only document I have available says the fuse is there and it's reflected somewhere on SRC.

 

best regards

0 项奖励
回复
1,105 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

This is true. Confirmed by support engineer.

 

Regards,

0 项奖励
回复
1,102 次查看
mastupristi
Senior Contributor I

Then I suggest removing the description of that fuse from both the Refernce Manual and the Security Refernece Manual

 

best regards

Max

0 项奖励
回复